CutSheetBuilder Class¶
-
class
NXOpen.Annotations.
CutSheetBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Builder for Formboard cut sheet functionality used in formboard.
This class queries and sets settings specific to formboard cut sheet.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AutoUpdate | Returns or sets the options specifies whether annotation automatically updates. |
FlattenHierarchy | Returns or sets the options specifies whether to flatten hierarchy. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AutoUpdate¶
-
CutSheetBuilder.
AutoUpdate
¶ Returns or sets the options specifies whether annotation automatically updates.
-------------------------------------
Getter Method
Signature
AutoUpdate
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoUpdate
Parameters: autoUpdate (bool) – New in version NX9.0.0.
License requirements: routing_harness (“Routing Harness”)
FlattenHierarchy¶
-
CutSheetBuilder.
FlattenHierarchy
¶ Returns or sets the options specifies whether to flatten hierarchy.
-------------------------------------
Getter Method
Signature
FlattenHierarchy
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlattenHierarchy
Parameters: flattenHierarchy (bool) – New in version NX9.0.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
Validate¶
-
CutSheetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.