CustomSymbolCollection Class¶
-
class
NXOpen.Annotations.
CustomSymbolCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.BaseCustomSymbol
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateCustomSymbol | Creates a custom symbol |
CreateDraftingCustomSymbolBuilder | Creates the Drafting Symbol placement builder |
CreateMasterSymbolBuilder | Creates the Master Symbol builder |
CreateMasterSymbolListItemBuilder | Creates the Master Symbol List Item builder |
CreatePmiCustomSymbol | Creates a PMI custom symbol |
CreatePmiCustomSymbolBuilder | Creates the PMI Symbol Placement builder |
CreateReplaceSymbolBuilder | Creates a NXOpen.Annotations.ReplaceSymbolBuilder |
CreateSmashCustomSymbolBuilder | Smashes a custom symbol |
CreateSymbolCatalogBuilder | Creates a symbol catalog dialog builder |
EditSymbolDisplayBuilder | Creates a edit custom symbol dialog builder |
FindObject | Finds the NXOpen.Annotations.MasterSymbol with the given name. |
NewCustomSymbolData | Creates new CustomSymbolData object |
NewPartSymbolData | Creates new CustomSymbolData object to create a part symbol instance. |
Method Detail¶
CreateCustomSymbol¶
-
CustomSymbolCollection.
CreateCustomSymbol
¶ Creates a custom symbol
Signature
CreateCustomSymbol(customSymbolData, origin, leader)
Parameters: - customSymbolData (
NXOpen.Annotations.CustomSymbolData
) – - origin (
NXOpen.Point3d
) – Origin for the custom symbol - leader (
NXOpen.Annotations.LeaderBundle
) – Specifies the leaders for the custom symbol
Returns: New custom symbol
Return type: New in version NX4.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DraftingCustomSymbolBuilder
instead.License requirements: drafting (“DRAFTING”)
- customSymbolData (
CreateDraftingCustomSymbolBuilder¶
-
CustomSymbolCollection.
CreateDraftingCustomSymbolBuilder
¶ Creates the Drafting Symbol placement builder
Signature
CreateDraftingCustomSymbolBuilder(symbolTag)
Parameters: symbolTag ( NXOpen.Annotations.CustomSymbol
) – Symbol as inputReturns: DraftingCustomSymbolBuilder object Return type: NXOpen.Annotations.DraftingCustomSymbolBuilder
New in version NX7.5.0.
License requirements: None.
CreateMasterSymbolBuilder¶
-
CustomSymbolCollection.
CreateMasterSymbolBuilder
¶ Creates the Master Symbol builder
Signature
CreateMasterSymbolBuilder(masterSymbolTag)
Parameters: masterSymbolTag ( NXOpen.Annotations.MasterSymbol
) –NXOpen.Annotations.MasterSymbol
to be set as master symbolReturns: MasterSymbolBuilder object Return type: NXOpen.Annotations.MasterSymbolBuilder
New in version NX7.5.0.
License requirements: None.
CreateMasterSymbolListItemBuilder¶
-
CustomSymbolCollection.
CreateMasterSymbolListItemBuilder
¶ Creates the Master Symbol List Item builder
Signature
CreateMasterSymbolListItemBuilder()
Returns: CustomSymbolListItemBuilder object Return type: NXOpen.Annotations.MasterSymbolListItemBuilder
New in version NX7.5.0.
License requirements: None.
CreatePmiCustomSymbol¶
-
CustomSymbolCollection.
CreatePmiCustomSymbol
¶ Creates a PMI custom symbol
Signature
CreatePmiCustomSymbol(customSymbolData, pmiData, annotationPlane, origin, leader)
Parameters: - customSymbolData (
NXOpen.Annotations.CustomSymbolData
) – - pmiData (
NXOpen.Annotations.PmiData
) – PMI data - annotationPlane (
NXOpen.Xform
) – Annotation plane on which the custom symbol lies - origin (
NXOpen.Point3d
) – Origin for the custom symbol - leader (
NXOpen.Annotations.LeaderBundle
) – Specifies the leaders for the custom symbol
Returns: New PMI custom symbol
Return type: New in version NX4.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.PmiCustomSymbolBuilder
instead.License requirements: geometric_tol (“GDT”)
- customSymbolData (
CreatePmiCustomSymbolBuilder¶
-
CustomSymbolCollection.
CreatePmiCustomSymbolBuilder
¶ Creates the PMI Symbol Placement builder
Signature
CreatePmiCustomSymbolBuilder(symbolTag)
Parameters: symbolTag ( NXOpen.Annotations.PmiCustomSymbol
) – Symbol as inputReturns: PMICustomSymbolBuilder object Return type: NXOpen.Annotations.PmiCustomSymbolBuilder
New in version NX7.5.0.
License requirements: None.
CreateReplaceSymbolBuilder¶
-
CustomSymbolCollection.
CreateReplaceSymbolBuilder
¶ Creates a
NXOpen.Annotations.ReplaceSymbolBuilder
Signature
CreateReplaceSymbolBuilder()
Returns: Return type: NXOpen.Annotations.ReplaceSymbolBuilder
New in version NX8.0.1.
License requirements: drafting (“DRAFTING”)
CreateSmashCustomSymbolBuilder¶
-
CustomSymbolCollection.
CreateSmashCustomSymbolBuilder
¶ Smashes a custom symbol
Signature
CreateSmashCustomSymbolBuilder()
Returns: Return type: NXOpen.Annotations.SmashCustomSymbolBuilder
New in version NX6.0.0.
License requirements: None.
CreateSymbolCatalogBuilder¶
-
CustomSymbolCollection.
CreateSymbolCatalogBuilder
¶ Creates a symbol catalog dialog builder
Signature
CreateSymbolCatalogBuilder()
Returns: Return type: NXOpen.Annotations.SymbolCatalogBuilder
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
EditSymbolDisplayBuilder¶
-
CustomSymbolCollection.
EditSymbolDisplayBuilder
¶ Creates a edit custom symbol dialog builder
Signature
EditSymbolDisplayBuilder(symbolTag)
Parameters: symbolTag ( NXOpen.Annotations.BaseCustomSymbol
) – Symbol as inputReturns: Return type: NXOpen.Annotations.EditSymbolDisplayBuilder
New in version NX7.5.0.
License requirements: None.
FindObject¶
-
CustomSymbolCollection.
FindObject
¶ Finds the
NXOpen.Annotations.MasterSymbol
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – Master custom symbol name Returns: Master custom symbol object Return type: NXOpen.Annotations.MasterSymbol
New in version NX7.5.0.
License requirements: None.
NewCustomSymbolData¶
-
CustomSymbolCollection.
NewCustomSymbolData
¶ Creates new CustomSymbolData object
Signature
NewCustomSymbolData(masterFileName)
Parameters: masterFileName (str) – Absolute path of the master symbol(with .sym.prt extension) Returns: New CustomSymbolData Return type: NXOpen.Annotations.CustomSymbolData
New in version NX4.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DraftingCustomSymbolBuilder
for Drafting Custom Symbol andNXOpen.Annotations.PmiCustomSymbolBuilder
for PMI Custom Symbol objects.License requirements: None.
NewPartSymbolData¶
-
CustomSymbolCollection.
NewPartSymbolData
¶ Creates new CustomSymbolData object to create a part symbol instance.
Signature
NewPartSymbolData(partSymbolName)
Parameters: partSymbolName (str) – Part symbol name. Part symbol is a master symbol that is created and instantiated in the same part. Returns: New CustomSymbolData Return type: NXOpen.Annotations.CustomSymbolData
New in version NX4.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DraftingCustomSymbolBuilder
for Drafting Custom Symbol andNXOpen.Annotations.PmiCustomSymbolBuilder
for PMI Custom Symbol objects.License requirements: None.