CompoundDatumReferenceBuilder Class¶
-
class
NXOpen.Annotations.
CompoundDatumReferenceBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.CompoundDatumReferenceBuilder
To create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreateCompoundDatumReferenceBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DatumReferenceList | Returns the list of datum references |
ExtendedText | Returns the compound datum reference extended text builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DatumReferenceList¶
-
CompoundDatumReferenceBuilder.
DatumReferenceList
¶ Returns the list of datum references
-------------------------------------
Getter Method
Signature
DatumReferenceList
Returns: Return type: NXOpen.Annotations.DatumReferenceBuilderList
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
ExtendedText¶
-
CompoundDatumReferenceBuilder.
ExtendedText
¶ Returns the compound datum reference extended text builder
-------------------------------------
Getter Method
Signature
ExtendedText
Returns: Return type: NXOpen.Annotations.TextWithSymbolsBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CompoundDatumReferenceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.