ChamferOrientationType Enumeration¶
-
class
NXOpen.Annotations.
ChamferOrientationType
¶ Bases:
object
Specifies the linear chamfer dimension orientation Enum Members
Enum Member Enum Member Description Horizontal default (same as the adjacent edge) Vertical perpendicular with default Parallel parallel to the chamfer line itself -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-