ChamferLeaderPlacement Enumeration¶
-
class
NXOpen.Annotations.
ChamferLeaderPlacement
¶ Bases:
object
Specifies the chamfer dimension leader placement relative to the chamfer Enum Members
Enum Member Enum Member Description Perpendicular Specifies leader perpendicular to the chamfer Parallel Specifies leader parallel to the chamfer Linear Specifies leader inline with the chamfer Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-