ChamferForm Enumeration¶
-
class
NXOpen.Annotations.
ChamferForm
¶ Bases:
object
Specifies the chamfer dimension form Enum Members
Enum Member Enum Member Description Symbol C5 Size 5 x 5 SizeAngle 5 x 45 AngleSize 45 x 5 Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-