CenterlineSettingsBuilder Class¶
-
class
NXOpen.Annotations.
CenterlineSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Builder for Centerline Settings.
This contains settings common to all centerlines .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of centerline |
Gap | Returns or sets the gap parameter for centeline |
Tag | Returns the Tag for this object. |
Width | Returns or sets the width of centerline |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CenterlineSettingsBuilderCenterlineThickness Enumeration | the types of centerline thickness |
Property Detail¶
Color¶
-
CenterlineSettingsBuilder.
Color
¶ Returns or sets the color of centerline
-------------------------------------
Getter Method
Signature
Color
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color
Parameters: color (Id) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Gap¶
-
CenterlineSettingsBuilder.
Gap
¶ Returns or sets the gap parameter for centeline
-------------------------------------
Getter Method
Signature
Gap
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Gap
Parameters: gap (float) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Width¶
-
CenterlineSettingsBuilder.
Width
¶ Returns or sets the width of centerline
-------------------------------------
Getter Method
Signature
Width
Returns: Return type: NXOpen.Annotations.CenterlineSettingsBuilderCenterlineThickness
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width
Parameters: width ( NXOpen.Annotations.CenterlineSettingsBuilderCenterlineThickness
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
CenterlineSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.