BillOfMaterialBuilderFabricationNumberingType Enumeration

NXOpen.Annotations.BillOfMaterialBuilder.FabricationNumberingType is an alias for NXOpen.Annotations.BillOfMaterialBuilderFabricationNumberingType

class NXOpen.Annotations.BillOfMaterialBuilderFabricationNumberingType

Bases: object

The options specify the fabrication numbering type.

Enum Members

Enum Member Enum Member Description
Sequential
Original
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.