BendTableSettingsBuilderColumnType Enumeration¶
NXOpen.Annotations.BendTableSettingsBuilder.ColumnType is an alias for NXOpen.Annotations.BendTableSettingsBuilderColumnType
-
class
NXOpen.Annotations.
BendTableSettingsBuilderColumnType
¶ Bases:
object
This enum represents the type of the column in the bend table
Enum Members
Enum Member Enum Member Description BendID Bend ID BendName Bend Name BendRadius Bend Radius BendAngle Bend Angle BendDirection Bend Direction IncludedAngle Included Angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-