BaseSurfaceFinishBuilderToleranceOption Enumeration¶
NXOpen.Annotations.BaseSurfaceFinishBuilder.ToleranceOption is an alias for NXOpen.Annotations.BaseSurfaceFinishBuilderToleranceOption
-
class
NXOpen.Annotations.
BaseSurfaceFinishBuilderToleranceOption
¶ Bases:
object
the valid surface finish tolerance types
Enum Members
Enum Member Enum Member Description NotSet No tolerance EqualBilateral Equal bilateral Bilateral Bilateral UnilateralPlus Unilateral plus UnilateralMinus Unilateral minus PlusLimitTwoLines Plus limit two lines MinusLimitTwoLines Minus limit two lines PlusLimitOneLine Plus limit one line MinusLimitOneLine Minus limit one line -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-