BaseSurfaceFinishBuilderParanthesesType Enumeration¶
NXOpen.Annotations.BaseSurfaceFinishBuilder.ParanthesesType is an alias for NXOpen.Annotations.BaseSurfaceFinishBuilderParanthesesType
-
class
NXOpen.Annotations.
BaseSurfaceFinishBuilderParanthesesType
¶ Bases:
object
the valid parantheses types. This enum is deprecated.
Deprecated since version NX8.0.0: Use
NXOpen.Annotations.BaseSurfaceFinishBuilderParenthesesType
instead.Enum Members
Enum Member Enum Member Description NotSet None Left Left Right Right Both Both -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-