BaseFrameBarBuilderAxisType Enumeration¶
NXOpen.Annotations.BaseFrameBarBuilder.AxisType is an alias for NXOpen.Annotations.BaseFrameBarBuilderAxisType
-
class
NXOpen.Annotations.
BaseFrameBarBuilderAxisType
¶ Bases:
object
Enum for Ship Axis This is used by
NXOpen.Annotations.BaseFrameBarBuilder.Axis()
andNXOpen.Annotations.BaseFrameBarBuilder.Axis()
to get/set the axis for a frame barEnum Members
Enum Member Enum Member Description X Ship X Axis Y Ship Y Axis Z Ship Z Axis -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-