AutomaticCenterlineBuilder Class¶
-
class
NXOpen.Annotations.
AutomaticCenterlineBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Automatic Centerlines
To create a new instance of this class, use
NXOpen.Annotations.CenterlineCollection.CreateAutomaticCenterlineBuilder()
Default values.
Property Value CylindricalExtension 1.5 (millimeters part), 0.0625 (inches part) InheritAngle 1 Width Thin New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color |
CylindricalExtension | Returns or sets the cylindrical extension |
InheritAngle | Returns or sets the inherit angle |
Tag | Returns the Tag for this object. |
Views | Returns the selected views |
Width | Returns or sets the width |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AutomaticCenterlineBuilderCenterlineThickness Enumeration | the types of centerline thickness |
Property Detail¶
Color¶
-
AutomaticCenterlineBuilder.
Color
¶ Returns or sets the color
-------------------------------------
Getter Method
Signature
Color
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color
Parameters: color (Id) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CylindricalExtension¶
-
AutomaticCenterlineBuilder.
CylindricalExtension
¶ Returns or sets the cylindrical extension
-------------------------------------
Getter Method
Signature
CylindricalExtension
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CylindricalExtension
Parameters: cylindricalExtension (float) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
InheritAngle¶
-
AutomaticCenterlineBuilder.
InheritAngle
¶ Returns or sets the inherit angle
-------------------------------------
Getter Method
Signature
InheritAngle
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritAngle
Parameters: inheritAngle (bool) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Views¶
-
AutomaticCenterlineBuilder.
Views
¶ Returns the selected views
-------------------------------------
Getter Method
Signature
Views
Returns: Return type: NXOpen.Drawings.SelectDraftingViewList
New in version NX6.0.0.
License requirements: None.
Width¶
-
AutomaticCenterlineBuilder.
Width
¶ Returns or sets the width
-------------------------------------
Getter Method
Signature
Width
Returns: Return type: NXOpen.Annotations.AutomaticCenterlineBuilderCenterlineThickness
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width
Parameters: width ( NXOpen.Annotations.AutomaticCenterlineBuilderCenterlineThickness
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
AutomaticCenterlineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.