AssociativityPointOption Enumeration¶
-
class
NXOpen.Annotations.
AssociativityPointOption
¶ Bases:
object
Specifies the associativity point option Enum Members
Enum Member Enum Member Description NotSet No point Control Control point ArcCenter Arc center point Tangent Tangent point Intersection Intersection point ScreenPosition Screen position OnCurve Point on curve Pole Spline pole Anchor Conic Anchor Defining Spline defining point Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-