AssociativityLineOption Enumeration¶
-
class
NXOpen.Annotations.
AssociativityLineOption
¶ Bases:
object
Specifies the associativity line option Enum Members
Linear
Bolt circle
Circular
- “
- “Angle”, “At angle” “HorizontalRight”, “Horizontal right” “VerticalUp”, “Vertical up” “HorizontalLeft”, “Horizontal left” “VerticalDown”, “Vertical down” “BaseLine”, “Base line” “Last”, “Last enum value. Should not be used.”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.