AssociativeTextPropertyType Enumeration¶
NXOpen.Annotations.AssociativeText.PropertyType is an alias for NXOpen.Annotations.AssociativeTextPropertyType
-
class
NXOpen.Annotations.
AssociativeTextPropertyType
¶ Bases:
object
the associative text property type to be used with the object
Enum Members
Enum Member Enum Member Description DrawingNumberOfSheets Drawing sheet number of sheets DrawingNumberOfPrimarySheets Drawing sheet number of primary sheets DrawingSheetName Drawing sheet name DrawingSheetNumber Drawing sheet number DrawingSheetRevision Drawing sheet revision DrawingSheetScaleNumerator Drawing sheet scale numerator DrawingSheetScaleDenominator Drawing sheet scale denominator DrawingSheetSize Drawing sheet size DrawingSheetUnits Drawing sheet units DrawingSheetZone Drawing sheet zone DrawingSheetProjectionAngle Drawing sheet projection angle DrawingMasterPartName Drawing master part name DrawingPartName Drawing part name DrawingViewPrefix Drawing view prefix DrawingViewRotationAngle View rotation angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-