AssociativeOriginType Enumeration

class NXOpen.Annotations.AssociativeOriginType

Bases: object

Specifies the type of associativity for an annotation’s origin Enum Members

Enum Member Enum Member Description
Drag
RelativeToView
RelativeToGeometry
VerticallyAligned
HorizontallyAligned
AlignedWithArrows
AtAPoint
OffsetFromText
AttachedToStack
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.