ArrowDisplay Enumeration¶
-
class
NXOpen.Annotations.
ArrowDisplay
¶ Bases:
object
Specifies the arrow display option Enum Members
Enum Member Enum Member Description Two Displays both the arrows First Displays arrow to the first object selected to create the dimension Second Displays arrow to the second object selected to create the dimension NotSet Doesn’t display arrows Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-