ArcComponent Class¶
-
class
NXOpen.Annotations.
ArcComponent
¶ Bases:
NXOpen.TransientObject
Represents a single arc in an annotation and can be queried for information about that arc.
This information includes the arc type, the start angle, the end angle, the radius, and the center point in absolute coordinates. .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
CenterPoint | Returns the arc center point in absolute coordinates. |
EndAngle | Returns the arc end angle in radians. |
Index | Returns the arc index. |
Radius | Returns the arc radius. |
StartAngle | Returns the arc start angle in radians. |
Type | Returns the arc type. |
Enumerations¶
ArcComponentArcType Enumeration | the arc type |
Property Detail¶
CenterPoint¶
-
ArcComponent.
CenterPoint
¶ Returns the arc center point in absolute coordinates.
If the annotation is on a drawing, the center point is returned in drawing space. If the annotation is on the model, the center point is returned in model space.
-------------------------------------
Getter Method
Signature
CenterPoint
Returns: the arc center point in absolute coordinates Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
EndAngle¶
-
ArcComponent.
EndAngle
¶ Returns the arc end angle in radians.
-------------------------------------
Getter Method
Signature
EndAngle
Returns: the arc end angle in radians Return type: float New in version NX6.0.0.
License requirements: None.
Index¶
-
ArcComponent.
Index
¶ Returns the arc index.
-------------------------------------
Getter Method
Signature
Index
Returns: the arc index Return type: int New in version NX9.0.0.
License requirements: None.
Radius¶
-
ArcComponent.
Radius
¶ Returns the arc radius.
-------------------------------------
Getter Method
Signature
Radius
Returns: the arc radius Return type: float New in version NX6.0.0.
License requirements: None.
StartAngle¶
-
ArcComponent.
StartAngle
¶ Returns the arc start angle in radians.
-------------------------------------
Getter Method
Signature
StartAngle
Returns: the arc start angle in radians Return type: float New in version NX6.0.0.
License requirements: None.
Type¶
-
ArcComponent.
Type
¶ Returns the arc type.
-------------------------------------
Getter Method
Signature
Type
Returns: the arc type Return type: NXOpen.Annotations.ArcComponentArcType
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
ArcComponent.
Dispose
¶ Free resources associated with the arc component.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.