AcisExporterAcisVersionOption Enumeration¶
NXOpen.AcisExporter.AcisVersionOption is an alias for NXOpen.AcisExporterAcisVersionOption
-
class
NXOpen.
AcisExporterAcisVersionOption
¶ Bases:
object
ACIS Version options
Enum Members
Enum Member Enum Member Description R26 R25 R24 R23 R22 R21 R20 R19 R18 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-