AMEBaseBuilder Class |
JA class for the insert Eng object dialog |
AMEBaseNode Class |
Represents Base Node |
AMEEngObject Class |
Represents Engineering Object |
AMEEngineeringObjectLabel Class |
Represents Engineering Object Label Object |
AMEExtendedObject Class |
Represents Extended Object |
AMEGroup Class |
Group Journaling class |
AMEGroupFolder Class |
Group Folder Journaling class |
AMEManager Class |
Represents a manager of automation designer objects |
AMENamingRule Class |
Represents Naming Rule Object |
AMEPlcHwItem Class |
Represents Plc Hw Item |
AMEPort Class |
Represents Port |
AMEQuery Class |
The Query Object |
AMEQueryGroup Class |
The Query Group |
AMEReportRule Class |
Represents Report Rule Object |
AccessorEvaluatorBuilder Class |
Evaluates an object based on a property value or an index |
AncestorEvaluatorBuilder Class |
Evaluates an ancestor for a given aspect and a starting point |
ApplicationBuilder Class |
Create the AD application builder see AMEApplicationBuilder |
AspectDetailsBuilder Class |
JA Class for the Aspect Details UI Block |
AspectNavigatorPreferencesBuilder Class |
JA class for aspect navigator builder |
AspectNode Class |
Aspect Node Journaling class |
AspectPrefixBuilder Class |
represents the builder class which is used to define Aspect Prefixes and Delimiter for NXOpen.AME.Project |
AspectRoot Class |
AspectRoot Node Journaling class |
AssignAspectBuilder Class |
Reassign a single aspect of an Engineering Object |
AssignSubnetBuilder Class |
Reassign a single aspect of an Engineering Object |
AssignTemplateToProductBuilder Class |
Builder class to assign a template object to NXOpen.AME.ProductDefinition |
AssignTypeBuilder Class |
Builder for selecting an engineering object definition |
AssignmentPort Class |
Represents AssignmentPort |
AttributeHolder Class |
JA class for the AttributeHolder object |
BaseDefinitionAttributeHolder Class |
BaseDefinition Atributes Holder Object |
BaseEvaluatorBuilder Class |
Represents the builder for all the evaluators. |
BasicPropertiesBuilder Class |
Represents a re-usable component for basic properties such as name and description |
BreakTemplateBuilder Class |
JA class for the insert Eng object dialog |
BulkConnectionBuilder Class |
builder for the bulk connection dialog |
BulkEngineeringObjectBuilder Class |
BulkEngineeringObjectBuilder class will be used for bulk Engineering Object Operation. |
CabinetComponentNode Class |
Cabinet Component Node class |
CabinetDesignBuilder Class |
the builder for creating cabinet design |
CabinetNode Class |
Cabinet Node class |
CabinetObject Class |
Cabinet Object class |
CabinetRoot Class |
Cabinet Root Node class |
CallMethodRuleBuilder Class |
JA class for the call method rule dialog |
ChildrenEvaluatorBuilder Class |
Evaluates the children objects for a given aspect and a starting point |
ConditionsBuilder Class |
JA class for the conditions dialog |
ConfigureResultTableBuilder Class |
Represents configure result table class builder |
ConnectToLibraryItemBuilder Class |
JA class for the connect to library item dialog |
ConnectedObjectsEvaluatorBuilder Class |
Evaluates the connected objects for the given port and a starting point |
CreateDefinitionBuilder Class |
Create and classify definition |
CreateEngObjectDefinitionBuilder Class |
Create and classify engineering object definition |
CreatePmiNoteBuilder Class |
Create PMINote dialog JA class |
CreateProductBuilder Class |
Create and classify product |
CreateTemplateBuilder Class |
Create Template dialog JA class |
CreateTemplateDefinitionBuilder Class |
Create and classify template definition |
DefineAspectBuilder Class |
Define Aspects for Engineering Object Definition |
DeviceFunctionDef Class |
Device Function Def class |
DiagramManager Class |
Represents an object that manages sheet elements. |
DocumentRoot Class |
Document Root Node class |
DocumentStructureBuilder Class |
Class to define Document Structure |
EClassClassNode Class |
EClassData Tree Node class |
EClassDataRoot Class |
EClassData Root Node class |
EClassFolderNode Class |
EClass Folder Node class |
EClassNode Class |
EClassData Tree Node class |
EClassObjectNode Class |
EClassData Tree Node class |
EClassSegmentNode Class |
EClass Segment Node class |
EClassVersionNode Class |
EClass Version Node class |
EOAttributeHolder Class |
EOAttributeHolder Atributes Holder Object |
EODataItemAttributeHolder Class |
EODef Atributes Holder Object |
EODefAttributeHolder Class |
EODef Atributes Holder Object |
EPLANPlug Class |
Represents EPLANPlug |
EPLANProjectSettings Class |
Eplan project settings Node Journaling class |
EPLANSocket Class |
Represents EPLANSocket |
EditAnnotationBuilder Class |
the builder for creating edit annotation |
EditClauseBuilder Class |
Naming Rule Builder |
EditEngineeringObjectBuilder Class |
JA class for the Eng object dialog |
EditOrderBuilder Class |
JA class for the Edit Order dialog |
EditQueryBuilder Class |
Edit Query Builder |
ElectricalAnnotationSettingsBuilder Class |
JA class for the Electrical Annotation Settings dialog |
ElectricalConnectionSettingsBuilder Class |
Builder object for changing electrical connection settings on diagramming pages associated with the NXOpen.AME.Project . |
EngineeringObjectAspectDetailBuilder Class |
JA class for the Engineering Object Aspect Detail UI block |
EngineeringObjectBaseBuilder Class |
JA class for the insert Eng object dialog |
EngineeringObjectBuilder Class |
JA class for the insert Eng object dialog |
EngineeringObjectDefinitionLabelBuilder Class |
JA class for the insert Engineering object definition label dialog |
EngineeringObjectNameBuilder Class |
JA class for the Engineering Object and Engineering Object def name and description superclass UI block |
EplanImportProjectTemplateBuilder Class |
EplanImportProjectTemplateBuilder |
EplanProjectGenerationBuilder Class |
the eplan project generation dialog builder |
EplanProjectTemplateAndStructureBuilder Class |
JA class for the Eplan project template dialog |
EplanSettingsBuilder Class |
EplanSettingsBuilder |
EplanStructureIdentifierOrderBuilder Class |
Represents a Eplan Structure identifier order Builder |
EplanStructureSettings Class |
Eplan structure settings Journaling class |
EvaluatorCopyToBuilder Class |
Copies evaluator and its dependents from one engineering object to another |
ExportEClassMappingBuilder Class |
Export eclass mapping into file |
ExpressionEvaluator Class |
Represents an Expression Evaluator |
ExtractAttribute Class |
Extract Attribute Journaling class |
ExtractAttributeAbsoluteBuilder Class |
Create a extract attribute |
ExtractAttributeBaseBuilder Class |
Create a extract attribute |
ExtractAttributeBuilder Class |
Create a extract attribute |
ExtractAttributeCurrentObjectBuilder Class |
Create a extract attribute |
ExtractAttributePortBuilder Class |
Create a extract port attribute builder |
ExtractAttributeRelativeBuilder Class |
Create a extract attribute |
FormSheetBuilder Class |
JA class for the Form Sheet dialog |
FormSheetObject Class |
JA class for the FormSheetObject |
FormSheetSettingsBuilder Class |
JA class for the Form Sheet Settings dialog |
FragmentAttributeHolder Class |
Fragment Object Atributes Holder |
FragmentBuilder Class |
Represents a Fragment creation class Builder |
FragmentObject Class |
Represents a Fragment Object |
FunctionCallInstanceBuilder Class |
JA class for the reuse rule dialog |
GeneralAnnotationSettingsBuilder Class |
builder for the general annotation settings dialog |
GeneralConnectionSettingsBuilder Class |
Builder for the General Connection Settings dialog |
GenerateReportsBuilder Class |
Comment |
GlobalSelectionBuilder Class |
GlobalSelectionBuilder |
GroupBuilder Class |
JA class for groups |
GroupRoot Class |
Group Root Node Journaling class |
IEngObject Class |
Represents Engineering Object |
IPort Class |
Represents an IPort |
IPortsContainer Class |
Represents Ports Container |
ImportEClassMappingBuilder Class |
Import eClass mapping |
ImportEClassProductBuilder Class |
Imports a eclass product xml file |
ImportEClassSchemaBuilder Class |
Imports a eclass schema xml file |
ImportEplanPageMacroBuilder Class |
ImportEplanPageMacroBuilder |
ImportGlobalMappingBuilder Class |
Imports a global mapping xml file |
ImportHWXmlBuilder Class |
the Import HW Xml builder |
ImportNode Class |
Import Object Journaling class |
ImportObject Class |
Import Object Journaling class |
InsertObjectBuilder Class |
JA class for Insert Object dialog |
InsertSettingsBuilder Class |
Re-usable UI for Settings properties in Insert EO and Insert Template dialog |
InstanceDataBlockBuilder Class |
JA class for the reuse rule dialog |
InstantiateBaseDefinitionReuseSelectionBuilder Class |
Builder for selecting base definition |
InstantiateTemplateBulkBuilder Class |
JA class for the insert Eng object dialog |
InterfaceMemberPort Class |
InterfaceMemberPort Journaling class |
InterruptionPointBuilder Class |
Represents builder for AME::DB::InterruptionPoint |
LDCachedAttribute Class |
JA class for the Line Design cache Attribute object |
LayoutDefinitionBuilder Class |
interface for the LayoutDefinitionBuilder |
LineDesignerMappingBuilder Class |
Line Designer mapping dialog JA interface |
LinkSymbolToDeviceTypeBuilder Class |
JA class for LinkSymbolToDeviceTypeBuilder dialog |
LoadLineDesignerBuilder Class |
JA class for the insert LoadLineDesigner dialog |
Manage2dSymbolsBuilder Class |
Represents a Manage2dSymbolsBuilder class Builder |
Manage3DModelsBuilder Class |
Represents the builder that is used to assign 3D models to a NXOpen.AME.ProductDefinition |
ManageEclassMappingBuilder Class |
Represents a ManageEclassMappingBuilder class Builder |
ManageObjectTypeBuilder Class |
Builder class for assigning AD type to NXOpen.Part and name to NXOpen.Assemblies.Component |
MapToExistingObjectBuilder Class |
Line Designer map to existing (EO) dialog JA interface |
MountingInterface Class |
Represents a Mounting Interface |
MountingInterfaceBuilder Class |
Builder class for creating mounting interface object in NXOpen.Part |
MultiValueObjectsPort Class |
MultiValueObjectsPort Journaling class |
MultipleObjectsBuilder Class |
JA class for the insert Eng object dialog |
NamingRuleBuilder Class |
Naming Rule Builder |
NamingRuleBuilderList Class |
Represents a list of objects. |
NamingRuleListBuilder Class |
Classification to Engineering Object Name Map Builder |
NamingRuleSettingsBuilder Class |
JA class for dialog for naming rule settings |
ObjectConnectionBuilder Class |
JA class for the reuse object connection block |
ObjectConnectionDetailBuilder Class |
JA class for the reuse object connection detail block |
ObjectEvaluatorBuilder Class |
Evaluates the object given a starting point |
ObjectNameBuilder Class |
Object Name JA class |
ObjectNameIndexBuilder Class |
Object Name Index JA class |
OperandRuleBuilder Class |
JA class for the parameter rule dialog |
OperatorRuleBuilder Class |
OperatorRule Dialog |
OpticalAnnotationSettingsBuilder Class |
JA class for the Optical Annotation Settings dialog |
OpticalConnectionSettingsBuilder Class |
Builder object for changing optical connection settings on diagramming pages associated with the NXOpen.AME.Project |
OrderAspectsBuilder Class |
Represents a OrderAspectsBuilder for changing the order of Navigator |
PageAttributeHolder Class |
Page Object Atributes Holder |
PageBuilder Class |
Represents a Page creation class Builder |
PageNamingBuilder Class |
Class to define Page naming schema |
PageNode Class |
Represents a Page Node |
PageObject Class |
Represents a Page Object |
ParameterRuleBuilder Class |
JA class for the parameter rule dialog |
ParentEvaluatorBuilder Class |
Evaluates the parent object for a given aspect and a starting point |
PlaceAutomationBuilder Class |
Reassign a single aspect of an Engineering Object |
PlcBlock Class |
Plc Block Node Journaling class |
PlcCodePosition Class |
Represents Plc Code Position Object |
PlcMemoryAreaBuilder Class |
Represents a Subnet creation class Builder |
PlcMethod Class |
Plc Method Node Journaling class |
PlcMethodBuilder Class |
The Journalling class for PlcMethodBuilder |
PlcRule Class |
PlcRule Journaling class |
PlcSoftwareGenPort Class |
PlcSoftwareGenPort Journaling class |
PlcSymbolBuilder Class |
Class to create Functional Tags and assign them to PLC Channels |
PlcSymbolsEvaluatorBuilder Class |
Evaluates the PLC tags for a given aspect and a starting point |
PlcVendorSymbolBuilder Class |
Represents a Subnet creation class Builder |
PortArtifact Class |
Represents a base class that provides common methods for port artifact in a NXOpen.PDM.ConditionalElementRevision . |
PortAttributeHolder Class |
Port Object Atributes Holder |
PortBuilder Class |
builder for the software block properties dialog |
PortConnectionBuilder Class |
builder for the port connector dialog |
PortEvaluatorBuilder Class |
Evaluates the port objects for the given port and a starting point |
PortsManagerBuilder Class |
Provides journal methods for the ports manager dialog. |
ProductComponent Class |
Product Component class |
ProductComponentInstance Class |
Product Component Instance class |
ProductDefAttributeHolder Class |
ProductDefinition Atributes Holder Object |
ProductDefinition Class |
JA class for the Product Definition object |
ProductDefinitionRoot Class |
Product Definition Root class |
ProductMatchingRulesBuilder Class |
Represents Product Matching Rules class builder |
ProductSelectionBuilder Class |
JA class for Product Selection dialog |
ProductSelectionDetailsBuilder Class |
Represents a Product Selection Details class Builder |
Project Class |
Project Journaling class |
ProjectEngineeringObjectBuilder Class |
JA class for the insert Project Eng object dialog |
PropertyEvaluatorBuilder Class |
Evaluates the property of an object given a category and property |
QueryBuilder Class |
Represents query class builder |
QueryClause Class |
JA class for the QueryClause object |
QueryFolder Class |
Query Folder Journaling class |
QueryNode Class |
The Query Node |
ReferenceDesignationSetNode Class |
Reference Designation Set Node Journaling class |
ReferenceObjectBuilder Class |
Re-usable UI consist of a context and source selection |
ReportTemplateBuilder Class |
Class to create Report Template and assign the ReportQuery and Report Layout to them |
ReportsSettingsBuilder Class |
interface for the ReportsSettingsBuilder |
SWStatusItem Class |
Represents SW Status Item |
SaveToLibraryBuilder Class |
Create Software Block JA class |
SchematicSymbol Class |
Represents a Schematic Symbol object |
SchematicSymbolConfigurationBuilder Class |
JA class for SchematicSymbolConfigurationBuilder dialog |
SelectAMEBaseNode Class |
Represents a single object selection. |
SelectAMEBaseNodeList Class |
Represents a list of objects on a selection list. |
SelectAMEExtendedObject Class |
Represents a single object selection. |
SelectAMEPort Class |
Represents a single object selection. |
SelectAndHighlightBuilder Class |
Represents a SelectAndHighlightBuilder for select and highlight in the Navigators |
SelectAspectNode Class |
Represents a single object selection. |
SelectBaseDefinitionNodeBuilder Class |
Builder for selecting base definition node from navigators |
SelectClassificationBuilder Class |
Select a part from the reuse library |
SelectClassificationFromTreeBuilder Class |
Select Type from the Classification Library |
SelectMountingInterfaceLocationBuilder Class |
Builder for selecting mounting interface location from graphics window |
SelectProductDefinitionBuilder Class |
JA class for the Product Definition Selection |
SelectProductOrEoDefinitionBuilder Class |
JA class for the Product Definition or Engineering Object Definition Selection |
SelectionBaseDefinitionBuilder Class |
Journalling Interface class for Builder which allows selection of BaseDefinition. |
SelectionEngineeringObjectDefinitionBuilder Class |
JA class for the Engineering Object Definition Block |
ShowHideObjectsBuilder Class |
JA class for ShowHideObjectsBuilder |
Snap3DModelsBuilder Class |
Represents a Snap3DModelsBuilder class Builder |
SortingBlockBuilder Class |
Sorts the list expression output according to the property |
SubnetBuilder Class |
Represents a Subnet creation class Builder |
SymbolAnnotationBuilder Class |
Represents a Symbol Annotation creation class Builder |
SymbolAnnotationSettingsBuilder Class |
JA class for the symbol settings |
SymbolAuthoringBuilder Class |
Represents a Symbol Authoring class Builder |
SymbolRoot Class |
Symbol Root Node class |
TCSavedQueriesBuilder Class |
Represents a TC Saved Queries builder |
TeeJunctionBuilder Class |
JA class for creating Tee Junction |
TiaPortalProjectSettings Class |
Tia Portal project settings node journaling class |
TiaPortalProjectSettingsBuilder Class |
TiaPortalProjectSettingsBuilder |
TiaProjectItemBuilder Class |
the TIA project item builder |
TransferFileDataBuilder Class |
Imports a new one or updates the existing configuration in AD Upstream Data Navigator from the external file. |
TypeMappingBuilder Class |
JA class for the type mapping dialog |
TypeMappingBuilderList Class |
Represents a list of objects. |
TypeMappingListBuilder Class |
Type Mapping List Builder |
UnloadLineDesignerBuilder Class |
JA class for the insert UnloadLineDesigner dialog |
UpstreamDataRoot Class |
UpstreamData Root Node class |