TeeJunctionBuilder Class¶
-
class
NXOpen.AME.
TeeJunctionBuilder
¶ Bases:
NXOpen.AME.AMEBaseBuilder
JA class for creating Tee Junction
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateTeeJunctionBuilder()
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetContextConnectionPortAndBendPoints | Set Context Connection’s Start Port and it’s Bend Points. |
SetLocation | Set Location of TeeJunction on Target Connection |
SetOwningSheet | Set TeeJunction’s owning sheet |
SetTargetConnection | Set Target Connection where TeeJunction must be created. |
SetTargetSegmentId | Set Target Connection’s segmentId |
SetTeeJunctionType | Set TeeJunction type. |
SetTeeJunctionVariant | Set TeeJunction variant. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
SetContextConnectionPortAndBendPoints¶
-
TeeJunctionBuilder.
SetContextConnectionPortAndBendPoints
¶ Set Context Connection’s Start Port and it’s Bend Points.
Signature
SetContextConnectionPortAndBendPoints(contextConnectionPort, p2dBendPoints)
Parameters: - contextConnectionPort (
NXOpen.AME.AMEExtendedObject
) – - p2dBendPoints (list of
NXOpen.Point2d
) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- contextConnectionPort (
SetLocation¶
-
TeeJunctionBuilder.
SetLocation
¶ Set Location of TeeJunction on Target Connection
Signature
SetLocation(locationX, locationY)
Parameters: - locationX (float) –
- locationY (float) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetOwningSheet¶
-
TeeJunctionBuilder.
SetOwningSheet
¶ Set TeeJunction’s owning sheet
Signature
SetOwningSheet(owningSheet)
Parameters: owningSheet ( NXOpen.Diagramming.Sheet
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetTargetConnection¶
-
TeeJunctionBuilder.
SetTargetConnection
¶ Set Target Connection where TeeJunction must be created.
Signature
SetTargetConnection(targetConnection)
Parameters: targetConnection ( NXOpen.Diagramming.Connection
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetTargetSegmentId¶
-
TeeJunctionBuilder.
SetTargetSegmentId
¶ Set Target Connection’s segmentId
Signature
SetTargetSegmentId(segmentID)
Parameters: segmentID (int) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetTeeJunctionType¶
-
TeeJunctionBuilder.
SetTeeJunctionType
¶ Set TeeJunction type.
Signature
SetTeeJunctionType(junctionType)
Parameters: junctionType ( NXOpen.AME.AmeTeeJunctionType
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetTeeJunctionVariant¶
-
TeeJunctionBuilder.
SetTeeJunctionVariant
¶ Set TeeJunction variant.
Signature
SetTeeJunctionVariant(variantIndex)
Parameters: variantIndex ( NXOpen.AME.AmeTeeJunctionVariant
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
TeeJunctionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.