SymbolAnnotationBuilderOrientation Enumeration¶
NXOpen.AME.SymbolAnnotationBuilder.Orientation is an alias for NXOpen.AME.SymbolAnnotationBuilderOrientation
-
class
NXOpen.AME.
SymbolAnnotationBuilderOrientation
¶ Bases:
object
Represents orientation of annotation
Enum Members
Enum Member Enum Member Description Horizontal Vertical -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-