ShowHideObjectsBuilder Class¶
-
class
NXOpen.AME.
ShowHideObjectsBuilder
¶ Bases:
NXOpen.Builder
JA class for ShowHideObjectsBuilder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateShowHideObjectsBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ShowChannels | Returns or sets the setting for showing/hiding Plc Channels in aspect navigators |
ShowEPLAN | Returns or sets the setting for showing/hiding EPLAN objects in aspect navigators |
ShowPlacedFragments | Returns or sets the setting for showing/hiding placed fragments in aspect navigators |
ShowSoftwareBlocks | Returns or sets the setting for showing/hiding software blocks in aspect navigators |
ShowTags | Returns or sets the setting for showing/hiding Plc Tags in aspect navigators |
ShowUnplacedFragments | Returns or sets the setting for showing/hiding the setting for unplaced fragments in aspect navigators |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ShowChannels¶
-
ShowHideObjectsBuilder.
ShowChannels
¶ Returns or sets the setting for showing/hiding Plc Channels in aspect navigators
-------------------------------------
Getter Method
Signature
ShowChannels
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowChannels
Parameters: showChannels (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowEPLAN¶
-
ShowHideObjectsBuilder.
ShowEPLAN
¶ Returns or sets the setting for showing/hiding EPLAN objects in aspect navigators
-------------------------------------
Getter Method
Signature
ShowEPLAN
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowEPLAN
Parameters: showEPLAN (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowPlacedFragments¶
-
ShowHideObjectsBuilder.
ShowPlacedFragments
¶ Returns or sets the setting for showing/hiding placed fragments in aspect navigators
-------------------------------------
Getter Method
Signature
ShowPlacedFragments
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowPlacedFragments
Parameters: showPlacedFragments (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowSoftwareBlocks¶
-
ShowHideObjectsBuilder.
ShowSoftwareBlocks
¶ Returns or sets the setting for showing/hiding software blocks in aspect navigators
-------------------------------------
Getter Method
Signature
ShowSoftwareBlocks
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowSoftwareBlocks
Parameters: showSoftwareBlocks (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowTags¶
-
ShowHideObjectsBuilder.
ShowTags
¶ Returns or sets the setting for showing/hiding Plc Tags in aspect navigators
-------------------------------------
Getter Method
Signature
ShowTags
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowTags
Parameters: showTags (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ShowUnplacedFragments¶
-
ShowHideObjectsBuilder.
ShowUnplacedFragments
¶ Returns or sets the setting for showing/hiding the setting for unplaced fragments in aspect navigators
-------------------------------------
Getter Method
Signature
ShowUnplacedFragments
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ShowUnplacedFragments
Parameters: showUnplacedFragments (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
ShowHideObjectsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.