PlcSymbolsEvaluatorBuilderFilterType Enumeration¶
NXOpen.AME.PlcSymbolsEvaluatorBuilder.FilterType is an alias for NXOpen.AME.PlcSymbolsEvaluatorBuilderFilterType
-
class
NXOpen.AME.
PlcSymbolsEvaluatorBuilderFilterType
¶ Bases:
object
choices for type filter, can either be tags, instance dbs, function blocks, functions, eplan macros, or all
Enum Members
Enum Member Enum Member Description Tags Idbs FunctionBlocks Functions PageMacros WindowMacros CallerInstance All -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-