PlcRuleType Enumeration¶
NXOpen.AME.PlcRule.Type is an alias for NXOpen.AME.PlcRuleType
-
class
NXOpen.AME.
PlcRuleType
¶ Bases:
object
replace or insert rule Type. Do not edit this enum!
Enum Members
Enum Member Enum Member Description SymbolicReference ConstantValue Variable LocalValue LocalVariable ConstantText Call SystemGlobalCall SystemLocalCall SystemFunctionCall UserLocalCall Method PlaceholderVariable PlaceholderSymbolicReference PlaceholderConstantValue OperatorAnd OperatorOr NotSet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-