PlcMemoryAreaBuilder Class¶
-
class
NXOpen.AME.
PlcMemoryAreaBuilder
¶ Bases:
NXOpen.Builder
Represents a Subnet creation class Builder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreatePlcMemoryAreaBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
DataLengthBit | Returns or sets the DataLengthBit |
DataLengthByte | Returns or sets the DataLengthByte |
Description | Returns or sets the Description |
IOType | Returns or sets the IOType |
Name | Returns or sets the Name |
StartAddress | Returns or sets the StartAddress |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DataLengthBit¶
-
PlcMemoryAreaBuilder.
DataLengthBit
¶ Returns or sets the DataLengthBit
-------------------------------------
Getter Method
Signature
DataLengthBit
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DataLengthBit
Parameters: dataLengthBit (int) – New in version NX12.0.0.
License requirements: None.
DataLengthByte¶
-
PlcMemoryAreaBuilder.
DataLengthByte
¶ Returns or sets the DataLengthByte
-------------------------------------
Getter Method
Signature
DataLengthByte
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DataLengthByte
Parameters: dataLengthByte (int) – New in version NX12.0.0.
License requirements: None.
Description¶
-
PlcMemoryAreaBuilder.
Description
¶ Returns or sets the Description
-------------------------------------
Getter Method
Signature
Description
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Description
Parameters: description (str) – New in version NX12.0.0.
License requirements: None.
IOType¶
-
PlcMemoryAreaBuilder.
IOType
¶ Returns or sets the IOType
-------------------------------------
Getter Method
Signature
IOType
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IOType
Parameters: ioType (str) – New in version NX12.0.0.
License requirements: None.
Name¶
-
PlcMemoryAreaBuilder.
Name
¶ Returns or sets the Name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX12.0.0.
License requirements: None.
StartAddress¶
-
PlcMemoryAreaBuilder.
StartAddress
¶ Returns or sets the StartAddress
-------------------------------------
Getter Method
Signature
StartAddress
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartAddress
Parameters: startAddress (int) – New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PlcMemoryAreaBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.