PlcDataType Enumeration¶
-
class
NXOpen.AME.
PlcDataType
¶ Bases:
object
Definition of the PLC data types
Enum Members
Enum Member Enum Member Description Db Fb Fc BlockDb BlockFb BlockFc BlockSdb BlockSfb BlockSfc BlockOb Bool Byte Char Counter Date Dint Dword Int Real S5time Time TimeOfDay Timer Word AomIdent ConnAny ConnOuc ConnPrg ConnRId DbAny DbDyn DbWww EventAny EventAtt EventHwint HwAny HwDevice HwDpmaster HwDpslave HwHsc HwIeport HwInterface HwIo HwIosystem HwModule HwPto HwPwm HwSubmodule Ldt Lint Lreal Ltime LtimeOfDay Lword ObAny ObAtt ObCyclic ObDelay ObDiag ObHwint ObPcycle ObStartup ObTimeerror ObTod Pip Port Rtm Sint Udint Uint Ulint Usint WChar Dtl Wstring Errorstruct IecCounter IecDcounter IecLcounter IecLtimer IecScounter IecTimer IecUcounter IecUdcounter IecUlcounter IecUscounter Cref Nref Vref HscPeriod TaddrParam SslHeader Conditions TconParam DateAndTime String Udt Any Struct Array Ob Variant Undefined Unknown -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-