PageNamingBuilder Class¶
-
class
NXOpen.AME.
PageNamingBuilder
¶ Bases:
NXOpen.Builder
Class to define Page naming schema
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreatePageNamingBuilder()
Default values.
Property Value DisplayDigits 1 Increment 1 Start 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DisplayDigits | Returns or sets the Display Digits |
Increment | Returns or sets the increment |
Start | Returns or sets the start name |
Tag | Returns the Tag for this object. |
TargetSelection | Returns the Target node selection |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DisplayDigits¶
-
PageNamingBuilder.
DisplayDigits
¶ Returns or sets the Display Digits
-------------------------------------
Getter Method
Signature
DisplayDigits
Returns: Return type: int New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
DisplayDigits
Parameters: displayDigits (int) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Increment¶
-
PageNamingBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment
Returns: Return type: int New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
Increment
Parameters: increment (int) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Start¶
-
PageNamingBuilder.
Start
¶ Returns or sets the start name
-------------------------------------
Getter Method
Signature
Start
Returns: Return type: int New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
Start
Parameters: start (int) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
TargetSelection¶
-
PageNamingBuilder.
TargetSelection
¶ Returns the Target node selection
-------------------------------------
Getter Method
Signature
TargetSelection
Returns: Return type: NXOpen.AME.SelectAMEBaseNode
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
PageNamingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.