ManageObjectTypeBuilder Class¶
-
class
NXOpen.AME.
ManageObjectTypeBuilder
¶ Bases:
NXOpen.Builder
Builder class for assigning AD type to
NXOpen.Part
and name toNXOpen.Assemblies.Component
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateManageObjectTypeBuilder()
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
AssignNewType | Assigns AD Type to input parts |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemoveType | Removes AD Type from input parts |
RenameComponent | Assigns new name to the input component |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AssignNewType¶
-
ManageObjectTypeBuilder.
AssignNewType
¶ Assigns AD Type to input parts
Signature
AssignNewType(parts, newType)
Parameters: - parts (list of
NXOpen.Part
) – - newType (str) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- parts (list of
RemoveType¶
-
ManageObjectTypeBuilder.
RemoveType
¶ Removes AD Type from input parts
Signature
RemoveType(parts)
Parameters: parts (list of NXOpen.Part
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
RenameComponent¶
-
ManageObjectTypeBuilder.
RenameComponent
¶ Assigns new name to the input component
Signature
RenameComponent(partOccurrence, name)
Parameters: - partOccurrence (
NXOpen.Assemblies.Component
) – - name (str) –
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- partOccurrence (
Validate¶
-
ManageObjectTypeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.