LoadLineDesignerBuilder Class¶
-
class
NXOpen.AME.
LoadLineDesignerBuilder
¶ Bases:
NXOpen.Builder
JA class for the insert LoadLineDesigner dialog
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateLoadLineDesignerBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
EnumRevisionRule | Returns or sets the revision rule |
Perimeter | Returns or sets the perimeter |
SelectionEngObject | Returns the selected objects |
Tag | Returns the Tag for this object. |
ToggleAdditionalObjects | Returns or sets the toggle for additional objects |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LoadLineDesignerBuilderRevisionRuleType Enumeration | enum for the revision rule |
Property Detail¶
EnumRevisionRule¶
-
LoadLineDesignerBuilder.
EnumRevisionRule
¶ Returns or sets the revision rule
-------------------------------------
Getter Method
Signature
EnumRevisionRule
Returns: Return type: NXOpen.AME.LoadLineDesignerBuilderRevisionRuleType
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
EnumRevisionRule
Parameters: enumRevisionRule ( NXOpen.AME.LoadLineDesignerBuilderRevisionRuleType
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Perimeter¶
-
LoadLineDesignerBuilder.
Perimeter
¶ Returns or sets the perimeter
-------------------------------------
Getter Method
Signature
Perimeter
Returns: Return type: float New in version NX11.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
Perimeter
Parameters: perimeter (float) – New in version NX11.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SelectionEngObject¶
-
LoadLineDesignerBuilder.
SelectionEngObject
¶ Returns the selected objects
-------------------------------------
Getter Method
Signature
SelectionEngObject
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ToggleAdditionalObjects¶
-
LoadLineDesignerBuilder.
ToggleAdditionalObjects
¶ Returns or sets the toggle for additional objects
-------------------------------------
Getter Method
Signature
ToggleAdditionalObjects
Returns: Return type: bool New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ToggleAdditionalObjects
Parameters: toggleAdditionalObjects (bool) – New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
LoadLineDesignerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.