InsertSettingsBuilder Class¶
-
class
NXOpen.AME.
InsertSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Re-usable UI for Settings properties in Insert EO and Insert Template dialog
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AspectPlacement | Returns or sets the aspect placement |
CopiesPerParent | Returns or sets the number of copies to insert per parent |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AspectPlacement¶
-
InsertSettingsBuilder.
AspectPlacement
¶ Returns or sets the aspect placement
-------------------------------------
Getter Method
Signature
AspectPlacement
Returns: Return type: bool New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
AspectPlacement
Parameters: aspectPlacement (bool) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
CopiesPerParent¶
-
InsertSettingsBuilder.
CopiesPerParent
¶ Returns or sets the number of copies to insert per parent
-------------------------------------
Getter Method
Signature
CopiesPerParent
Returns: Return type: int New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
CopiesPerParent
Parameters: copiesPerParent (int) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
InsertSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.