ExtractAttributeBuilder Class¶
-
class
NXOpen.AME.
ExtractAttributeBuilder
¶ Bases:
NXOpen.Builder
Create a extract attribute
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateExtractAttributeBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AbsoluteAttributeBuilder | Returns the absolute attribute builder |
CurrentObjectAttributeBuilder | Returns the current object attribute builder |
ExtractType | Returns or sets the object type extraction |
PortAttributeBuilder | Returns the port attribute builder |
RelativeAttributeBuilder | Returns the relative attribute builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExtractAttributeBuilderType Enumeration | extract type Type |
Property Detail¶
AbsoluteAttributeBuilder¶
-
ExtractAttributeBuilder.
AbsoluteAttributeBuilder
¶ Returns the absolute attribute builder
-------------------------------------
Getter Method
Signature
AbsoluteAttributeBuilder
Returns: Return type: NXOpen.AME.ExtractAttributeAbsoluteBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
CurrentObjectAttributeBuilder¶
-
ExtractAttributeBuilder.
CurrentObjectAttributeBuilder
¶ Returns the current object attribute builder
-------------------------------------
Getter Method
Signature
CurrentObjectAttributeBuilder
Returns: Return type: NXOpen.AME.ExtractAttributeCurrentObjectBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ExtractType¶
-
ExtractAttributeBuilder.
ExtractType
¶ Returns or sets the object type extraction
-------------------------------------
Getter Method
Signature
ExtractType
Returns: Return type: NXOpen.AME.ExtractAttributeBuilderType
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
-------------------------------------
Setter Method
Signature
ExtractType
Parameters: type ( NXOpen.AME.ExtractAttributeBuilderType
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
PortAttributeBuilder¶
-
ExtractAttributeBuilder.
PortAttributeBuilder
¶ Returns the port attribute builder
-------------------------------------
Getter Method
Signature
PortAttributeBuilder
Returns: Return type: NXOpen.AME.ExtractAttributePortBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
RelativeAttributeBuilder¶
-
ExtractAttributeBuilder.
RelativeAttributeBuilder
¶ Returns the relative attribute builder
-------------------------------------
Getter Method
Signature
RelativeAttributeBuilder
Returns: Return type: NXOpen.AME.ExtractAttributeRelativeBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
ExtractAttributeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.