EplanStructureIdentifierOrderBuilder Class¶
-
class
NXOpen.AME.
EplanStructureIdentifierOrderBuilder
¶ Bases:
NXOpen.Builder
Represents a Eplan Structure identifier order Builder
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateEplanStructureIdentifierOrderBuilder()
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFunctionIdentifierOrder | The structure order index for function |
GetLocationIdentifierOrder | The structure order index for location |
GetObject | Returns the object currently being edited by this builder. |
SetFunctionIdentifierOrder | The structure order index for function |
SetLocationIdentifierOrder | The structure order index for location |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateStructureIdentifierOrder | Update structure identifier order. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetFunctionIdentifierOrder¶
-
EplanStructureIdentifierOrderBuilder.
GetFunctionIdentifierOrder
¶ The structure order index for function
Signature
GetFunctionIdentifierOrder()
Returns: Return type: list of str New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetLocationIdentifierOrder¶
-
EplanStructureIdentifierOrderBuilder.
GetLocationIdentifierOrder
¶ The structure order index for location
Signature
GetLocationIdentifierOrder()
Returns: Return type: list of str New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetFunctionIdentifierOrder¶
-
EplanStructureIdentifierOrderBuilder.
SetFunctionIdentifierOrder
¶ The structure order index for function
Signature
SetFunctionIdentifierOrder(rowStrings)
Parameters: rowStrings (list of str) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetLocationIdentifierOrder¶
-
EplanStructureIdentifierOrderBuilder.
SetLocationIdentifierOrder
¶ The structure order index for location
Signature
SetLocationIdentifierOrder(rowStrings)
Parameters: rowStrings (list of str) – New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
UpdateStructureIdentifierOrder¶
-
EplanStructureIdentifierOrderBuilder.
UpdateStructureIdentifierOrder
¶ Update structure identifier order.
Signature
UpdateStructureIdentifierOrder()
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
EplanStructureIdentifierOrderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.