ConditionsBuilder Class¶
-
class
NXOpen.AME.
ConditionsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
JA class for the conditions dialog
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
RemoveCondition | Remove the condition for the rule |
SetCondition | Set the condition for the rule |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
RemoveCondition¶
-
ConditionsBuilder.
RemoveCondition
¶ Remove the condition for the rule
Signature
RemoveCondition()
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetCondition¶
-
ConditionsBuilder.
SetCondition
¶ Set the condition for the rule
Signature
SetCondition(exp)
Parameters: exp ( NXOpen.Expression
) –New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
ConditionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.