BusInterfaceType Enumeration¶
-
class
NXOpen.AME.
BusInterfaceType
¶ Bases:
object
Bus Interface type. NOTE: order is important (is TIA order), please don’t change it
Enum Members
Enum Member Enum Member Description ProfibusDp Mpi Profinet AsInterface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-