NXOpen .NET Reference
12.0.0
|
Provides classes and interfaces for the NX Open Common API. More...
Namespaces | |
package | AME |
Provides classes and interfaces for AME. | |
package | Annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations. | |
package | Assemblies |
Provides classes and interfaces for Assemblies. | |
package | BlockStyler |
Provides classes and interfaces for Block Styler. | |
package | BodyDes |
Provides classes and interfaces for Body Design. | |
package | CAE |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation. | |
package | CAM |
Provides classes and interfaces for Manufacturing. | |
package | Diagramming |
Provides classes and interfaces relating to Diagramming. | |
package | DiagrammingLibraryAuthor |
Provides classes and interfaces for Diagramming Library Authoring. | |
package | Die |
Provides classes and interfaces relating to Die Engineering and Die Design. | |
package | Display |
Provides classes and interfaces for Display. | |
package | DMU |
Provides classes and interfaces for DMU. | |
package | Drafting |
Provides classes and interfaces for the Drafting. | |
package | Drawings |
Provides classes and interfaces for Drafting Drawings. | |
package | Facet |
Provides classes and interfaces for Faceted Representations. | |
package | Features |
Provides classes and interfaces for features. | |
package | Fields |
Provides classes and interfaces for Fields. | |
package | Formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality. | |
package | Gateway |
Provides classes and interfaces for Gateway. | |
package | GeometricAnalysis |
Provides classes and interfaces for Geometric Analysis. | |
package | GeometricUtilities |
Provides classes and interfaces for Geometric Utilities. | |
package | Issue |
Provides classes and interfaces for Issue Management. | |
package | Layer |
Provides classes and interfaces for layer. | |
package | Layout2d |
Provides classes and interfaces for Layout2D. | |
package | LineDesigner |
Provides classes and interfaces for Line Designer. | |
package | Markup |
Provides classes and interfaces for Markup. | |
package | MechanicalRouting |
Provides classes and interfaces for Mechanical Routing. | |
package | Mechatronics |
Provides classes and interfaces for Mechatronics. | |
package | MenuBar |
Provides classes and interfaces for the Menu Bar. | |
package | Mfg |
Provides classes and interfaces for Manufacturing. | |
package | MfgModel |
Provides classes and interfaces for Manufacturing Model. | |
package | ModlDirect |
Provides classes and interfaces for Direct Modeling. | |
package | ModlUtils |
Provides classes and interfaces for ModlUtils. | |
package | Motion |
Provides classes and interfaces for Motion Simulation. | |
package | OpenXml |
Provide classes and interfaces for OpenXml. | |
package | Optimization |
Provides classes and interfaces for Optimization. | |
package | Options |
Provides classes and interfaces for options. | |
package | PartFamily |
Provides classes and interfaces for Part Family. | |
package | PDM |
Provides classes and interfaces for PDM. | |
package | PhysMat |
Provides classes and interfaces for Physical Material. | |
package | PID |
Provides classes and interfaces for PID. | |
package | Placement |
Provides classes and interfaces for Placement. | |
package | PLAS |
Provides classes and interfaces for PLAS. | |
package | Positioning |
Provides classes and interfaces for Assembly Positioning and Constraints. | |
package | Preferences |
Provides classes and interfaces for preferences. | |
package | PressLineSimulation |
Provides classes and interfaces for Press Line Simulation. | |
package | Report |
Provides classes and interfaces for Report. | |
package | Routing |
Provides classes and interfaces for Routing. | |
package | ShapeSearch |
Provides classes and interfaces for Shape Search. | |
package | SheetMetal |
Provides classes and interfaces for Sheet Metal. | |
package | ShipDesign |
Provides classes and interfaces for Ship Design. | |
package | SIM |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation. | |
package | ToolDesigner |
Provides classes and interfaces for ToolDesigner. | |
package | Tooling |
Provides classes and interfaces for Tooling. | |
package | UF |
Provides classes and interfaces to the UF API. | |
package | UIStyler |
Provides classes and interfaces for User Interface Styler. | |
package | UserDefinedObjects |
Provides classes and interfaces for User Defined Objects (UDOs). | |
package | UserDefinedTemplate |
Provides classes and interfaces for User Defined Template. | |
package | Utilities |
Provides classes and interfaces for Utilities. | |
package | Validate |
Provides classes and interfaces for Validation Utilities. | |
package | VectorArithmetic |
Provides classes and interfaces for Vector Arithmetic. | |
package | VisualReporting |
Provides classes and interfaces for Visual Reporting. | |
package | Weld |
Provides classes and interfaces for Weld. | |
Classes | |
class | AcisExporter |
Represents a AcisExporter to be used when importing the Acis Data This class is created using DexManager . More... | |
class | AcisImporter |
Represents a AcisImporter to be used when importing the Acis Data This class is created using DexManager . More... | |
class | ApparentChainingRule |
Represents a NXOpen.SelectionIntentRule that collects curves which appear connected or tangent connected in a particular drafting view. More... | |
class | Arc |
Represents an arc curve. More... | |
class | ArcCollection |
Represents a collection of arcs. More... | |
class | ASCImporter |
Represents a NXOpen.ASCImporter . More... | |
class | AssembliesUtils |
Contains various assembly utility methods More... | |
class | AttributeIterator |
This class is used to iterate over the user attributes of an object, with options to restrict or extend such searches More... | |
class | AttributeManager |
Provides methods for querying and updating attributes. More... | |
class | AttributePropertiesBaseBuilder |
Represents an NXOpen.AttributePropertiesBaseBuilder to be used for creating attributes. More... | |
class | AttributePropertiesBuilder |
Represents an NXOpen.AttributePropertiesBuilder . More... | |
class | AttributeTemplatesBuilder |
Represents an NXOpen.AttributeTemplatesBuilder to be used when creating attribute templates. More... | |
class | AutomaticTraceline |
Represents an automatic traceline. More... | |
class | Axis |
Represents an NXOpen.Axis class. More... | |
class | AxisCollection |
Represents a collection of NXOpen.Axis . More... | |
class | BasePart |
Base class for an NX part. More... | |
class | BasePropertyTable |
Represents a property table More... | |
class | BasicEffectivityBuilder |
Represent an interface class for basic effectivity block to assign or edit discrete effectivity unit values. More... | |
class | Body |
Represents a Body More... | |
class | BodyCollection |
Represents a collection of bodies in a part More... | |
class | BodyDumbRule |
Represents a NXOpen.SelectionIntentRule that collects bodies without any intent i. More... | |
class | BodyFacetsRule |
Represents a NXOpen.FacetSelectionRule that collects all facets from a Face Body. More... | |
class | BodyFeatureRule |
Represents a NXOpen.SelectionIntentRule that collects all bodies created or modified by a feature. More... | |
class | BodyGroupRule |
Represents a NXOpen.SelectionIntentRule that collects all bodies of a group. More... | |
class | BodyList |
Represents a list of objects. More... | |
class | BrushFacetsRule |
Represents a NXOpen.FacetSelectionRule that collects facets with brush tool intent. More... | |
class | Builder |
A Builder is an object that is used to create and edit other objects. More... | |
class | BunchFacetsOnFaceRule |
Represents a NXOpen.FacetSelectionRule that collects all facets from a face or a NX faceted body. More... | |
class | CaeObjectType |
Represent options for CAE selection. More... | |
class | CartesianCoordinateSystem |
Represents a cartesian coordinate system More... | |
class | Catiav4Creator |
Represents a NXOpen.Catiav4Creator to be used when exporting the CATIA V4 Data This class is created using NXOpen.DexManager . More... | |
class | Catiav4Importer |
Represents a NXOpen.Catiav4Importer to be used when importing the CATIA V4 Data This class is created using NXOpen.DexManager . More... | |
class | Catiav5Creator |
Represents a NXOpen.Catiav5Creator to be used when exporting the CATIA V5 Data This class is created using NXOpen.DexManager . More... | |
class | Catiav5Importer |
Represents a NXOpen.Catiav5Importer to be used when importing the CATIA V5 Data This class is created using NXOpen.DexManager . More... | |
class | CDF |
Represents a NXOpen.CDF , which is a representation of an NX color palette. More... | |
class | CGMBuilder |
Represents a NXOpen.CGMBuilder to be used when exporting the Current Display or drawing sheets to a CGM. More... | |
class | CGMImporter |
Used to import a CGM file into the work part. More... | |
class | ClipboardOperationsManager |
Used to create importer objects. More... | |
class | CollaborativeContentManager |
Represents the manager for the various collaborative design contents and this class is usable only when NX is running in managed mode. More... | |
class | CollaborativeDesign |
A collaborative design is created in Teamcenter. More... | |
class | CollaborativeDesignCollection |
A collection of collaborative designs. More... | |
struct | ColorDefinitionRgb |
Specifies rgb values for color More... | |
class | ColorDefinition |
Represents a NXOpen.ColorDefinition , which is a representation of one color on an NX color palette. More... | |
class | ColorManager |
Contains functionality pertaining to colors More... | |
class | ColorRegionRule |
Represents a NXOpen.FacetSelectionRule that chains to collect all connected facets of same color. More... | |
class | ColorWidth |
Represents a NXOpen.ColorWidth used by NXOpen.WidthDefinition to define a custom width for each color. More... | |
class | Conic |
Represents a conic curve. More... | |
class | ContentDefinition |
Represents a class that defines the contents that will be pulled in to a subset. More... | |
class | ConvergentFacet |
Represents a facet from convergent topology. More... | |
class | ConvertToFromReferenceBuilder |
Represents a NXOpen.ConvertToFromReferenceBuilder More... | |
class | CoordinateSystem |
Represents a coordinate system More... | |
class | CoordinateSystemCollection |
Represents a collection of NXOpen.CoordinateSystem . More... | |
class | Curve |
Represents a curve. More... | |
class | CurveChainRule |
Represents a NXOpen.SelectionIntentRule that collects end-to-end connected curves from the seed curve. More... | |
class | CurveCollection |
Represents a collection of NXOpen.Curve . More... | |
class | CurveDumbRule |
Represents a NXOpen.SelectionIntentRule that collects curves without any intent i. More... | |
class | CurveFeatureChainRule |
Represents a NXOpen.SelectionIntentRule that collects end-to-end connected curves from the feature of the seed. More... | |
class | CurveFeatureRule |
Represents a NXOpen.SelectionIntentRule that collects all curves created by a feature. More... | |
class | CurveFeatureTangentRule |
Represents a NXOpen.SelectionIntentRule that collects tangent connected curves from the feature of the seed. More... | |
class | CurveGroupRule |
Represents a NXOpen.SelectionIntentRule that collects all curves of a group. More... | |
class | CurveTangentRule |
Represents a NXOpen.SelectionIntentRule that collects tangent connected curves from the seed curve. More... | |
class | CustomPopupMenu |
Represents Custom Popup Menu Item class More... | |
class | CustomPopupMenuHandler |
Represents Custom Popup Menu Handler class More... | |
class | CustomPopupMenuItem |
Represents Custom Popup Menu Item class More... | |
class | CustomWidth |
Represents a NXOpen.CustomWidth used by NXOpen.WidthDefinition to define the three custom widths associated with each WidthDefinition. More... | |
class | CutView |
Represents a Cut View More... | |
class | CutViewCollection |
Represents a collection of NXOpen.CutView objects. More... | |
class | CylindricalCoordinateSystem |
Represents a cylindrical coordinate system More... | |
class | DataContainer |
Represents a list of data. More... | |
class | DateBuilder |
The DateBuilder class allows a date and/or time to be input or output via the DateItem builder. More... | |
class | DateItemBuilder |
This class stores a date and time. More... | |
class | DateItemBuilderList |
Represents a list of objects. More... | |
class | DatumAxis |
Represents a datum axis More... | |
class | DatumCollection |
Represents a collection of datum geometry. More... | |
class | DatumConstraint |
Represents a constraint that specifies the location of a NXOpen.Features.DatumFeature . More... | |
class | DatumPlane |
Represents a datum plane More... | |
class | Decal |
Represents a Material Texture decal pair More... | |
class | DexBuilder |
This is an abstract class that provides the basic functionality common to all dex builders. More... | |
class | DexManager |
The DexManager class provides methods to create Dex Builder objects. More... | |
class | Direction |
Represents a direction. More... | |
class | DirectionCollection |
Represents a collection of NXOpen.Direction . More... | |
class | DisplayableObject |
Base class for all objects that are displayable. More... | |
class | DisplayManager |
Represents an object to manage display settings. More... | |
class | DisplayModification |
Represents changes to the display characteristics of an object. More... | |
class | DraftingManager |
Represents an object that manages drafting objects and member views. More... | |
class | DraftPointDataCollection |
This class contains the factory methods for creating a DraftPointData object. More... | |
class | DrawingCompareManager |
Represents an object that manages drawing compare. More... | |
class | DrawingUtils |
Contains various drawing utility methods More... | |
class | DxfdwgCreator |
Represents a NXOpen.DxfdwgCreator to be used when exporting the DXF/DWG Data This class is created using NXOpen.DexManager . More... | |
class | DxfdwgImporter |
Represents a NXOpen.DxfdwgImporter to be used when importing the DXF/DWG Data This class is created using NXOpen.DexManager . More... | |
class | Edge |
Represents an edge More... | |
class | EdgeBodyRule |
Represents a NXOpen.SelectionIntentRule that collects all the edges of a body. More... | |
class | EdgeBoundaryRule |
Represents a NXOpen.SelectionIntentRule that collects all the edges of a face. More... | |
class | EdgeChainRule |
Represents a NXOpen.SelectionIntentRule that collects end-to-end connected edges from the body of the seed edge. More... | |
class | EdgeDumbRule |
Represents a NXOpen.SelectionIntentRule that collects edges without any intent i. More... | |
class | EdgeFaceRule |
Represents a NXOpen.SelectionIntentRule that collects all edges of a face. More... | |
class | EdgeFeatureRule |
Represents a NXOpen.SelectionIntentRule that collects all edges created or modified by a feature. More... | |
class | EdgeIntersectRule |
Represents a NXOpen.SelectionIntentRule that collects all intersection edges between a set of faces. More... | |
class | EdgeMultipleSeedTangentRule |
Represents a NXOpen.SelectionIntentRule that collects tangent connected edges from the body of the seed edge. More... | |
class | EdgeSheetBoundaryRule |
Represents a NXOpen.SelectionIntentRule that collects boundary edges of a sheet body. More... | |
class | EdgeTangentRule |
Represents a NXOpen.SelectionIntentRule that collects tangent connected edges from the body of the seed edge. More... | |
class | EdgeVertexRule |
Represents a NXOpen.SelectionIntentRule that collects the vertex edge and and its adjacent edges. More... | |
class | EdgeVertexTangentRule |
Represents a NXOpen.SelectionIntentRule that collects the vertex edge and the edges adjacent and tangent to it. More... | |
class | EffectivityConditionBuilder |
Represent a utility class to assign or edit discrete and range effectivity unit values in the context of a NXOpen.CollaborativeDesign . More... | |
class | Ellipse |
Represents an ellipse curve. More... | |
class | EllipseCollection |
Represents a collection of ellipses. More... | |
class | EndCutBlockBuilder |
Represents a End Cut Block Builder. More... | |
class | EngineeringFunction |
Contains Engineering Function methods More... | |
class | ErrorInfo |
Contains information about an error that occurred More... | |
class | ErrorList |
Represents a list of errors More... | |
class | Expression |
Represents an expression. More... | |
class | ExpressionCollection |
Represents a collection of expressions. More... | |
class | ExpressionCollectorSet |
An object that binds an expression with an entity section in the context of a list. More... | |
class | ExpressionCollectorSetList |
Represents a list of objects. More... | |
class | ExpressionGroup |
Represents an expression group. More... | |
class | ExpressionGroupCollection |
Represents a collection of expressions groups. More... | |
class | ExpressionSectionSet |
An object that binds an expression with an entity section in the context of a list. More... | |
class | ExpressionSectionSetList |
Represents a list of objects. More... | |
class | Face |
Represents a face More... | |
class | FaceAdjacentRule |
Represents a NXOpen.SelectionIntentRule that collects the faces adjacent to the seed face of a body. More... | |
class | FaceAllBlendRule |
Represents a NXOpen.SelectionIntentRule that collects all blend faces. More... | |
class | FaceAndAdjacentFacesRule |
Represents a NXOpen.SelectionIntentRule that collects both the seed face and all its adjacent faces. More... | |
class | FaceBodyRule |
Represents a NXOpen.SelectionIntentRule that collects all the faces of a body. More... | |
class | FaceBossPocketFacesRule |
Represents a NXOpen.SelectionIntentRule that collects all faces of a boss or pocket. More... | |
class | FaceConnectedBlendRule |
Represents a NXOpen.SelectionIntentRule that collects all connected blend faces. More... | |
class | FaceDumbRule |
Represents a NXOpen.SelectionIntentRule that collects faces without any intent i. More... | |
class | FaceFacetsRule |
Represents a NXOpen.FacetSelectionRule that collects all facets from a face or NX facet body. More... | |
class | FaceFeatureRule |
Represents a NXOpen.SelectionIntentRule that collects all faces created or modified by a feature. More... | |
class | FaceMergedRibFacesRule |
Represents a NXOpen.SelectionIntentRule that collects all merged rib faces. More... | |
class | FaceRegionBoundaryRule |
Represents a NXOpen.SelectionIntentRule that collects a region of faces that are tangent connected. More... | |
class | FaceRegionRule |
Represents a NXOpen.SelectionIntentRule that collects a region of faces. More... | |
class | FaceRibFacesRule |
Represents a NXOpen.SelectionIntentRule that collects all rib faces. More... | |
class | FaceSlotFacesRule |
Represents a NXOpen.SelectionIntentRule that collects all faces of a pocket. More... | |
class | FaceTangentRule |
Represents a NXOpen.SelectionIntentRule that collects tangent connected faces from the body of the seed face. More... | |
class | FacetCollector |
Represents collection of facets More... | |
class | FacetCollectorCollection |
This class contains the factory method for creating a facet collector. More... | |
class | FacetSelectionRule |
Represents a NXOpen.FacetSelectionRule facet collection rules. More... | |
class | FacetSelectionRuleFactory |
This class contains the factory methods for creating facet selection intent rules More... | |
class | FeatureGeneralPropertiesBuilder |
Represents a NXOpen.FeatureGeneralPropertiesBuilder to be used for modifying the names of features and general objects. More... | |
class | FeatureIntersectionEdgesRule |
Represents a NXOpen.SelectionIntentRule that collects the intersection edges of boolean like features. More... | |
class | FeaturePointsRule |
Represents a NXOpen.SelectionIntentRule that collects all points created by a feature. More... | |
class | FeatureProcessBuilderStatus |
More... | |
class | FileNew |
Represents a NXOpen.FileNew More... | |
class | FillBoundaryRule |
Represents a NXOpen.FacetSelectionRule that collects flood filled facets without doing any check of facet's existence in current collection. More... | |
class | FineBrushFacetsRule |
Represents a NXOpen.FacetSelectionRule that collects facets with fine brush tool intent. More... | |
class | FlatteningBuilder |
Represents a FlatteningBuilder builder. More... | |
class | FloodFillFacetsRule |
Represents a NXOpen.FloodFillFacetsRule that collects flood filled facets. More... | |
class | FollowFilletRule |
Represents a NXOpen.SelectionIntentRule that collects curves/edges which are connected or tangent connected and follow onto and off an untrimmed fillet. More... | |
class | FontCollection |
Represents a collection of typographical fonts (for example, Arial, OldEnglish) More... | |
class | FourPointSurfaceBuilder |
Represents a four point sheet body builder More... | |
class | GeneralScalarTable |
Represents a General M x N table of scalar (real) values. More... | |
class | GenericMeasure |
Represents a single valued measurement More... | |
class | Group |
Represents a gateway group More... | |
class | GroupBuilder |
Represents a NXOpen.GroupBuilder More... | |
class | HumanData |
Represent the data used to create the human More... | |
class | HumanHandsDialogBuilder |
Dialog for creating and editing standalone/"disembodied" hand figures More... | |
class | HumanHandShapeData |
Represent hand shape data More... | |
class | HumanPosturePrediction |
Represent posture prediction object More... | |
class | HumanPosturePredictionBuilder |
Represents a Human Posture Prediction Builder. More... | |
class | HumanReachZone |
Represents a human reach zone. More... | |
class | Hyperbola |
Represents a hyperbola curve. More... | |
class | HyperbolaCollection |
Represents a collection of hyperbolas. More... | |
interface | IAttributeSourceObjectBuilder |
Represents an interface to perform various database operations on an array of NXOpen.NXObject . More... | |
interface | IBaseCurve |
Represents something containing a two dimensional curve More... | |
interface | IBasePlane |
Represents a Plane or Datum Plane More... | |
interface | IBody |
Represents something containing a body More... | |
interface | ICurve |
Represents something containing a two dimensional modeling curve More... | |
class | IFacet |
Represents a facet. More... | |
interface | IFitTo |
Represents something that can be supplied to View.FitToObjects More... | |
class | IgesCreator |
Represents a NXOpen.IgesCreator to be used when exporting the IGES Data This class is created using NXOpen.DexManager . More... | |
class | IgesImporter |
Represents a NXOpen.IgesImporter to be used when importing the IGES Data This class is created using NXOpen.DexManager . More... | |
interface | ILocation |
Represents something that can be supplied to an location selection More... | |
class | Importer |
Base class for importing data into the work part. More... | |
class | ImportManager |
Used to create importer objects. More... | |
class | InferredConstraintsBuilder |
Represents a NXOpen.InferredConstraintsBuilder More... | |
class | InferSnapType |
Represent options for snap selection. More... | |
class | InfiniteLine |
Represents a infinite line curve. More... | |
class | InfiniteLineCollection |
Represents a collection of infinite lines. More... | |
class | Information |
Represents a class that provides methods for displaying information about part history, interpart parents and children, features, points, and other NX Objects. More... | |
class | InterpartExpressionsBuilder |
This class creates interpart expressions from the source part to the current work part via the naming rule defined. More... | |
interface | INXObject |
Represents an interface from which most NXOpen classes inherit More... | |
interface | IOrientation |
Represents something that can be supplied to an orientation selection More... | |
interface | IParameterizedSurface |
Represents something containing a face More... | |
interface | IPlane |
Represents an Plane class. More... | |
interface | IProfile |
Represents something that can be supplied to a profile More... | |
interface | IReferenceAxis |
Represents an object that could be used as a reference axis for a feature More... | |
interface | ISketchHelpedConstraint |
Represents a sketch constraint that has a help point or help parameter. More... | |
interface | ISurface |
Represents something containing a two dimensional surface More... | |
interface | ITableEditorDataProvider |
Interface for providing basic data for a Table Editor block. More... | |
class | ItemCacheMappedEntityBuilder |
Generic journal methods for ItemCacheMappedEntityBuilder More... | |
class | JournalManager |
Represents the JournalManager which is used to query data about journals when recording and replaying journal files. More... | |
class | JtCreator |
Represents a NXOpen.JtCreator to be used when exporting the JT Data This class is created using NXOpen.PvtransManager . More... | |
class | KFObject |
Represents an KF object in the part. More... | |
class | Layout |
Represents a layout. More... | |
class | LayoutCollection |
Represents a collection of layouts. More... | |
class | LayoutDefinition |
Represents the definition of a layout. More... | |
class | LicenseManager |
Provides utility methods for managing licenses. More... | |
class | Light |
Represents a light source. More... | |
class | LightCollection |
Represents a collection of NXOpen.Light s. More... | |
class | Line |
Represents a line curve. More... | |
class | LineCollection |
Represents a collection of lines. More... | |
class | LineColorFontWidthBuilder |
Represent a NXOpen.LineColorFontWidthBuilder More... | |
class | LineFontBuilder |
Represent a NXOpen.LineFontBuilder More... | |
class | LineWidthBuilder |
Represents a NXOpen.LineWidthBuilder More... | |
class | LinkedMirrorPartAttributeEditData |
JA interface for LinkedMirrorPartAttributeEditData object More... | |
class | LinkedMirrorPartAttributeEditEvent |
JA interface for LinkedMirrorPartAttributeEditEvent object More... | |
class | LinkedMirrorPartBuilder |
builder class of LinkedMirrorPartBuilder More... | |
class | LinkedMirrorPartEntityMapData |
JA interface for LinkedMirrorPartEntityMapData oject More... | |
class | LinkedMirrorPartEntityMapEvent |
JA interface for LinkedMirrorPartEntityMapEvent object More... | |
class | LinkedPartManager |
Represents the customization interface during linked mirror part creation and update. More... | |
class | ListCreator |
Represents a NXOpen.ListCreator to be used when exporting the JT Data This class is created using NXOpen.PvtransManager . More... | |
class | ListCreatorList |
Represents a list of objects. More... | |
class | ListingWindow |
Represents a ListingWindow. More... | |
class | LoadOptions |
Contains accessor methods for all the part load options. More... | |
class | LogFile |
Represents the system log file More... | |
class | MassPropertiesBuilder |
Represents a NXOpen.MassPropertiesBuilder for calculating the weight of selected objects as well as informing the part that the assemblies weight property data needs to be updated on save. More... | |
class | Material |
Represents Material More... | |
class | MaterialManager |
A manager to deal with all material objects More... | |
class | MaterialUtilities |
Represents Physical NXOpen.MaterialUtilities class More... | |
class | MathUtils |
Contains various math utility methods More... | |
class | Measure |
Represents a measurement feature More... | |
class | MeasureAngle |
Represents a single valued Angle measurement More... | |
class | MeasureAngleBuilder |
Represents a NXOpen.MeasureAngleBuilder More... | |
class | MeasureBodies |
Represents the measurement specific mass properties for a set of bodies More... | |
class | MeasureBodyBuilder |
Represents a NXOpen.MeasureBodyBuilder More... | |
class | MeasureBuilder |
Represents a NXOpen.MeasureBuilder More... | |
class | MeasureDistance |
Represents a single valued distance measurement More... | |
class | MeasureDistanceBuilder |
Represents a NXOpen.MeasureDistanceBuilder More... | |
class | MeasureFaceBuilder |
Represents a NXOpen.MeasureFaceBuilder More... | |
class | MeasureFaces |
Represents the measurement of perimeter and area of a set of faces More... | |
class | MeasureLength |
Represents a single valued length measurement More... | |
class | MeasureManager |
Provides methods for manipulating the measurement objects in a part. More... | |
class | Measurement |
Provides methods for calculating and displaying the measurement information. More... | |
class | MeasurePoint |
Represents a point measurement More... | |
class | MeasurePolarAngle |
Represents a single valued polar angle measurement More... | |
class | MeasurePolarArea |
Represents a single valued polar area measurement More... | |
class | MeasurePolarRadius |
Represents a single valued polar radius measurement More... | |
class | MeasureRectangularExtreme |
Represents a rectangular extreme point measurement More... | |
class | MeshParameterData |
Represents surface rebuild data structure. More... | |
class | MeshProfileString |
Represents Mesh profile string More... | |
class | ModelingView |
Represents a Modeling View More... | |
class | ModelingViewCollection |
Represents a collection of ModelingView s. More... | |
class | ModelingViewHighQualityImage |
Represents the properties and methods for generating a High Quality Image of a Modeling View More... | |
class | ModelingViewList |
Represents a list of objects. More... | |
class | MovieManager |
Represents a MovieManager class. More... | |
class | MovieSettingsBuilder |
This class is the builder for the Movie Settings. More... | |
class | MWUpdate |
Update tools used in Mold Wizard for the Journamation layer More... | |
class | NavigatorFilter |
Represents a NXOpen.NavigatorFilter object. More... | |
class | NXColor |
Represents a standard NX color. More... | |
class | NxFacet |
Represents a facet from convergent topology. More... | |
class | NXMatrix |
Represents an NX matrix. More... | |
class | NXMatrixCollection |
Represents a collection of NX Matrixes. More... | |
class | NXMessageBox |
Displays message box. More... | |
class | NXObject |
A base class providing low-level services for most NXOpen classes. More... | |
class | NXObjectList |
Represents a list of objects. More... | |
class | NamespaceDoc |
Provides classes and interfaces for the NX Open Common API. More... | |
class | NXTo2dCreator |
Represents a NXOpen.NXTo2dCreator to be used when exporting the 2D Data This class is created using NXOpen.DexManager . More... | |
class | ObjectGeneralPropertiesBuilder |
Represents an NXOpen.ObjectGeneralPropertiesBuilder to be used for modifying the names and properties of objects. More... | |
class | ObjectList |
Represents a list of objects. More... | |
class | ObjectSelector |
Represents a NXOpen.ObjectSelector to be used when exporting the the selected objects from NX part. More... | |
class | ObjectTypeSelector |
Represents a NXOpen.ObjectTypeSelector to be used when filter out the objects based on the type during import/export. More... | |
class | Offset |
Represents a NXOpen.Offset . More... | |
class | OffsetCollection |
Represents a collection of NXOpen.Offset . More... | |
class | OuterEdgesOfFacesRule |
Represents a NXOpen.SelectionIntentRule that collects the outer edges of a group of faces. More... | |
class | Parabola |
Represents a parabola curve. More... | |
class | ParabolaCollection |
Represents a collection of Parabolas More... | |
class | Part |
Represents an NX part of type .prt. More... | |
class | PartCleanup |
Provides utilities to to eliminate certain inaccessible objects from the part file. More... | |
class | PartCloseResponses |
Manages a list of part name/response pairs which are used to determine whether a part should be closed if modified during part close. More... | |
class | PartCloseStatus |
This class represents a list of part names with associated status codes that serve to communicate why these parts were not able to be closed. More... | |
class | PartCollection |
Represents the collection of all parts in a session. More... | |
class | PartDelayedUpdateStatus |
Represents a list of part names with associated delay status codes. More... | |
class | PartFamilyManager |
This class represents part family More... | |
class | PartFamilyMemberData |
This class is responsible for storing part family member data Use the method NXOpen.Part.NewPartFamilyMemberData to create new instance of this class. More... | |
class | PartFamilyMemberValues |
This class is responsible for storing part family member attribute values. More... | |
class | PartImporter |
Used to import a part into the work part. More... | |
class | PartLoadStatus |
Represents a list of part names with associated status codes. More... | |
class | PartReopenReport |
Contains information about a part and its components after it has been reopened. More... | |
class | PartReopenStatus |
Contains information about a part after an attempt was made to reopen it. More... | |
class | PartSaveOptions |
Contains accessor methods for all part save options that follow the part. More... | |
class | PartSaveStatus |
This class represents a list of part names with associated status codes that serve to communicate why these parts where not able to be saved during part save. More... | |
class | PasteSpecialBuilder |
Represents a NXOpen.PasteSpecialBuilder More... | |
class | PhysicalMaterial |
Represents Physical Material More... | |
class | PhysicalMaterialBuilder |
Represents a NXOpen.PhysicalMaterial builder More... | |
class | PhysicalMaterialCollection |
Represents the collection of all NXOpen.PhysicalMaterial objects in this Part More... | |
class | Plane |
Represents an Plane class. More... | |
class | PlaneCollection |
Represents a collection of NXOpen.Plane . More... | |
class | PlaneList |
Represents a list of objects. More... | |
class | PlaneTypes |
Represents an NXOpen.PlaneTypes class. More... | |
class | PlotBuilder |
Represents a NXOpen.PlotBuilder . More... | |
class | PlotColorsWidthsBuilder |
Represents a NXOpen.PlotColorsWidthsBuilder to be used for plotting. More... | |
class | PlotManager |
The PlotManager class provides methods to create Gateway Builder objects. More... | |
class | PlotSourceBuilder |
Represents a NXOpen.PlotSourceBuilder More... | |
class | Point |
Represents a smart Point . More... | |
class | PointCollection |
Represents a collection of smart NXOpen.Point . More... | |
class | PointList |
Represents a list of objects. More... | |
class | PolygonModelingTaskEnvironment |
Represents the Polygon Modeling task environment associated with a session. More... | |
class | Polyline |
Represents a polyline curve. More... | |
class | PolylineCollection |
Represents a collection of polylines. More... | |
class | PositioningDimension |
Represents a dimension object attached to the feature More... | |
class | PreviewPropertiesBuilder |
Represents a NXOpen.PreviewPropertiesBuilder to be used for creating and storing previews. More... | |
class | Print3dBuilder |
This class sends the 3d model for 3dprinting. More... | |
class | PrintBuilder |
Represents a NXOpen.PrintBuilder . More... | |
class | PrintPDFBuilder |
Represents a NXOpen.PrintPDFBuilder to be used when exporting the Current Display or selected sheets to a PDF document. More... | |
class | ProeImporter |
Represents a NXOpen.ProeImporter to be used when importing the ProE Data This class is created using NXOpen.DexManager . More... | |
class | PropertiesManager |
The PropertiesManager class provides methods to create Gateway Properties Builder objects. More... | |
class | PropertyContainer |
Represents a list of properties. More... | |
class | PvtransManager |
The PvtransManager class provides methods to create Pvtrans Builder objects. More... | |
class | ReferenceSet |
Represents a NXOpen.ReferenceSet . More... | |
class | RegionBoundaryRule |
Represents a NXOpen.SelectionIntentRule that collects curves as specified by an enclosed region. More... | |
class | RegionPoint |
Represents a point and body context on a region point. More... | |
class | RegionPointList |
Represents a list of objects. More... | |
class | RemoteUtilities |
This class is primarily designed for use in a remote session, and allows client applications to access resources on a remote server. More... | |
class | ReplaceExpressionsBuilder |
This class creates Replace expressions from the source part to the current work part via the naming rule defined. More... | |
class | RibTopFaceEdgesRule |
Represents a NXOpen.SelectionIntentRule that collects the like convexity outer edges of a group of faces. More... | |
class | RoughBrushFacetsRule |
Represents a NXOpen.FacetSelectionRule that collects facets with rough brush tool intent. More... | |
class | RuleManager |
Provides methods for manipulating the Knowledge Fusion rules in a part. More... | |
class | SaveOptions |
Contains accessor methods for all part save options that follow the session. More... | |
class | Scalar |
Represents a scalar. More... | |
class | ScalarCollection |
Represents a collection of NXOpen.Scalar objects. More... | |
class | ScalarMatrixValue |
Represents a General M x N matrix of scalar (real) values. More... | |
class | ScalarTableValue |
Represents a General M x N table of scalar (real) values. More... | |
class | ScCollector |
Represents a collector More... | |
class | ScCollectorCollection |
This class contains the factory methods for creating a sc collector. More... | |
class | ScCollectorList |
Represents a list of objects. More... | |
class | ScRuleFactory |
This class contains the factory methods for creating selection intent rules More... | |
class | Section |
Represents a section More... | |
class | SectionCollection |
This class contains the factory methods for creating a section. More... | |
class | SectionData |
Represents section data More... | |
class | SectionElementData |
Represents section element data More... | |
class | SectionList |
Represents a list of objects. More... | |
class | SelectBody |
Represents a single object selection. More... | |
class | SelectBodyList |
Represents a list of objects on a selection list. More... | |
class | SelectCartesianCoordinateSystem |
Represents a single object selection. More... | |
class | SelectCoordinateSystem |
Represents a single object selection. More... | |
class | SelectCoordinateSystemList |
Represents a list of objects on a selection list. More... | |
class | SelectCurve |
Represents a single object selection. More... | |
class | SelectCurveList |
Represents a list of objects on a selection list. More... | |
class | SelectDatumPlane |
Represents a single object selection. More... | |
class | SelectDatumPlaneList |
Represents a list of objects on a selection list. More... | |
class | SelectDisplayableObject |
Represents a single object selection. More... | |
class | SelectDisplayableObjectList |
Represents a list of objects on a selection list. More... | |
class | SelectEdge |
Represents a single object selection. More... | |
class | SelectEdgeList |
Represents a list of objects on a selection list. More... | |
class | SelectExpressionList |
Represents a list of objects on a selection list. More... | |
class | SelectFace |
Represents a single object selection. More... | |
class | SelectFaceList |
Represents a list of objects on a selection list. More... | |
class | SelectGroup |
Represents a single object selection. More... | |
class | SelectIBaseCurve |
Represents a single object selection. More... | |
class | SelectIBaseCurveList |
Represents a list of objects on a selection list. More... | |
class | SelectIBasePlaneList |
Represents a list of objects on a selection list. More... | |
class | SelectIBody |
Represents a single object selection. More... | |
class | SelectICurve |
Represents a single object selection. More... | |
class | SelectICurveList |
Represents a list of objects on a selection list. More... | |
class | SelectINXObjectList |
Represents a list of objects on a selection list. More... | |
class | Selection |
Defines an interface object for executing selection operations More... | |
class | SelectionHandle |
Represents a SelectionHandle for UI Styler More... | |
class | SelectionIntentRule |
Represents a NXOpen.SelectionIntentRule which essentially provides capabilities to collect curves, edges, faces and bodies. More... | |
class | SelectionMethod |
Represents the output from a smart selector method More... | |
class | SelectionSubscriber |
Defines a SelectionSubscriber for managing selection events More... | |
class | SelectIParameterizedSurface |
Represents a single object selection. More... | |
class | SelectIParameterizedSurfaceList |
Represents a list of objects on a selection list. More... | |
class | SelectIReferenceAxis |
Represents a single object selection. More... | |
class | SelectISurface |
Represents a single object selection. More... | |
class | SelectLine |
Represents a single object selection. More... | |
class | SelectModelingViewList |
Represents a list of objects on a selection list. More... | |
class | SelectNXObject |
Represents a single object selection. More... | |
class | SelectNXObjectList |
Represents a list of objects on a selection list. More... | |
class | SelectObject |
Represents a single object selection. More... | |
class | SelectObjectList |
Represents a list of objects on a selection list. More... | |
class | SelectPart |
Represents a single object selection. More... | |
class | SelectPartList |
Represents a list of objects on a selection list. More... | |
class | SelectPoint |
Represents a single object selection. More... | |
class | SelectPointList |
Represents a list of objects on a selection list. More... | |
class | SelectSketch |
Represents a single object selection. More... | |
class | SelectSmartObject |
Represents a single object selection. More... | |
class | SelectSpline |
Represents a single object selection. More... | |
class | SelectSplineList |
Represents a list of objects on a selection list. More... | |
class | SelectTaggedObject |
Represents a single object selection. More... | |
class | SelectTaggedObjectList |
Represents a list of objects on a selection list. More... | |
class | SelectView |
Represents a single object selection. More... | |
class | SelectViewList |
Represents a list of objects on a selection list. More... | |
class | Session |
Represents the NX session. More... | |
class | SingleFacetRule |
Represents a NXOpen.FacetSelectionRule that collects facets without any intent i. More... | |
class | SingleMeasure |
Represents a single valued measurement More... | |
class | Sketch |
Represents a sketch More... | |
class | SketchAlignmentConstraint |
Represents a sketch alignment constraint More... | |
class | SketchAlongPathBuilder |
Use the NXOpen.SketchAlongPathBuilder to create or reattach a NXOpen.Sketch along a path. More... | |
class | SketchAngularDimensionBuilder |
Represents a NXOpen.SketchAngularDimensionBuilder More... | |
class | SketchAssociativeTrim |
Represents a sketch associative trim constraint More... | |
class | SketchAssociativeTrimBuilder |
Represents a NXOpen.SketchAssociativeTrimBuilder More... | |
class | SketchAutoConstrainBuilder |
Represents a NXOpen.SketchAutoConstrainBuilder More... | |
class | SketchAutoDimensionBuilder |
Represents a NXOpen.SketchAutoDimensionBuilder More... | |
class | SketchChamferBuilder |
Represents a Chamfer builder More... | |
class | SketchCollection |
Represents a collection of sketches More... | |
class | SketchConicBuilder |
Represents a NXOpen.SketchConicBuilder builder More... | |
class | SketchConstraint |
Represents a constraint in a sketch. More... | |
class | SketchConstraintBuilder |
Represents a NXOpen.SketchConstraint builder More... | |
class | SketchCornerBuilder |
Create a corner between two sketch curves. More... | |
class | SketchDimensionalConstraint |
Represents a dimensional constraint More... | |
class | SketchDimensionBuilder |
Edit the geometry references of an existing sketch dimension. More... | |
class | SketchEditDefiningSectionBuilder |
Represents a NXOpen.SketchEditDefiningSectionBuilder builder. More... | |
class | SketchEllipseBuilder |
Represents a NXOpen.SketchEllipseBuilder builder More... | |
class | SketchEvaluator |
Represents a sketch-on-path evaluator. More... | |
class | SketchEvaluatorCollection |
Represents a collection of NXOpen.SketchEvaluator . More... | |
class | SketchExpressionModifierBuilder |
Represents a Sketch Expression Modifier Builder. More... | |
class | SketchG1Constraint |
Represents a sketch G1 constraint More... | |
class | SketchG2Constraint |
Represents a sketch G2 constraint More... | |
class | SketchGeometricConstraint |
Represents a geometric sketch constraint More... | |
class | SketchHelpedDimensionalConstraint |
Represents a dimensional sketch constraint that has a help point or help parameter More... | |
class | SketchHelpedGeometricConstraint |
Represents a geometric sketch constraint that has a help point or help parameter More... | |
class | SketchInDraftingBuilder |
Use the NXOpen.SketchInDraftingBuilder to create a NXOpen.Sketch on a NXOpen.Drawings.DraftingView or NXOpen.Drawings.DrawingSheet . More... | |
class | SketchInPlaceBuilder |
Use the NXOpen.SketchInPlaceBuilder to create or reattach a NXOpen.Sketch on a NXOpen.DatumPlane or planar NXOpen.Face . More... | |
class | SketchIntersectionCurve |
Represents a Intersection Curve operation inside sketch More... | |
class | SketchIntersectionCurveBuilder |
Represents a NXOpen.SketchIntersectionCurve builder More... | |
class | SketchIntersectionPoint |
Represents an Intersection Point operation inside sketch More... | |
class | SketchIntersectionPointBuilder |
Represents a NXOpen.SketchIntersectionPoint builder More... | |
class | SketchLinearDimensionBuilder |
Represents a NXOpen.SketchLinearDimensionBuilder More... | |
class | SketchMakeSymmetricBuilder |
This class is used to add symmetric contraint to objects from a NXOpen.SketchMakeSymmetricBuilder . More... | |
class | SketchMirrorPatternBuilder |
Represents a NXOpen.SketchMirrorPatternBuilder More... | |
class | SketchOffset |
Represents a sketch offset constraint More... | |
class | SketchOffsetBuilder |
Represents a NXOpen.SketchOffsetBuilder More... | |
class | SketchPasteBuilder |
Represents a NXOpen.SketchPasteBuilder More... | |
class | SketchPattern |
Represents a sketch pattern constraint More... | |
class | SketchPatternBuilder |
Represents a NXOpen.SketchPatternBuilder More... | |
class | SketchPolygon |
Represents a polygon constraint in a sketch More... | |
class | SketchPolygonBuilder |
Represents a NXOpen.SketchPolygon builder More... | |
class | SketchProjectBuilder |
Represents a NXOpen.SketchProjectBuilder builder More... | |
class | SketchQuickExtendBuilder |
Represents a NXOpen.SketchQuickExtendBuilder More... | |
class | SketchQuickTrimBuilder |
Represents a NXOpen.SketchQuickTrimBuilder More... | |
class | SketchRadialDimensionBuilder |
Represents a NXOpen.SketchRadialDimensionBuilder More... | |
class | SketchRapidDimensionBuilder |
Represents a NXOpen.SketchRapidDimensionBuilder More... | |
class | SketchTangentConstraint |
Represents a tangent constraint More... | |
class | SketchTangentToStringConstraint |
Represents a sketch tangent to string constraint More... | |
class | SmartObject |
Represents a smart object. More... | |
class | SphericalCoordinateSystem |
Represents a spherical coordinate system More... | |
class | Spline |
Represents a spline curve. More... | |
class | SplineCollection |
Represents a collection of splines. More... | |
class | Spreadsheet |
Represents a class for internal spreadsheet. More... | |
class | SpreadsheetCellData |
Represents a class for Spreadsheet cell data. More... | |
class | SpreadsheetExternal |
Represents a class for external spreadsheet. More... | |
class | SpreadsheetManager |
Represents a class for interacting with spreadsheets. More... | |
class | Step203Creator |
Represents a NXOpen.Step203Creator to be used when exporting the STEP203 Data This class is created using NXOpen.DexManager . More... | |
class | Step203Importer |
Represents a NXOpen.Step203Importer to be used when importing the STEP203 Data This class is created using NXOpen.DexManager . More... | |
class | Step214Creator |
Represents a NXOpen.Step214Creator to be used when exporting the STEP214 Data This class is created using NXOpen.DexManager . More... | |
class | Step214Importer |
Represents a NXOpen.Step214Importer to be used when importing the STEP214 Data This class is created using NXOpen.DexManager . More... | |
class | Step242Importer |
Represents a NXOpen.Step242Importer to be used when importing STEP242 Data This class is created using NXOpen.DexManager . More... | |
class | StepCreator |
Represents a NXOpen.StepCreator to be used when exporting the STEP Data This class is created using NXOpen.DexManager . More... | |
class | STLCreator |
Represents a NXOpen.STLCreator to be used when exporting the STL Data This class is created using NXOpen.DexManager . More... | |
class | STLImporter |
Used to import an STL file into the work part. More... | |
class | SubdivisionMeshBody |
Represents a subdivision mesh. More... | |
class | SubdivisionMeshEdge |
Represents a subdivision mesh edge. More... | |
class | SubdivisionMeshFace |
Represents a subdivision mesh face. More... | |
class | SubdivisionMeshVertex |
Represents a subdivision mesh vertex. More... | |
class | SubdivisionTaskEnvironment |
Represents the subdivision task environment associated with a session. More... | |
class | SuppressByExpressionBuilder |
Represents a NXOpen.SuppressByExpressionBuilder More... | |
class | SurfaceRebuildData |
Represents surface rebuild data structure. More... | |
class | SurfaceUVDirectionBuilder |
Represents an edit surface u/v direction builder that allows reversing or swapping parametric directions. More... | |
class | SymbolFont |
Represents a symbol font More... | |
class | TableEditorDefaultDataProvider |
Provides basic data for a Table Editor block. More... | |
class | TaggedObjectList |
Represents a list of objects. More... | |
class | TextColorFontWidthBuilder |
Represent a NXOpen.TextColorFontWidthBuilder More... | |
class | Traceline |
Represents a traceline. More... | |
class | TracelineCollection |
Represents a collection of tracelines More... | |
class | TreeListNode |
Represents a TreeList Node Object More... | |
struct | Point3d |
Represents three-dimensional cartesian coordinates for a point More... | |
struct | Vector3d |
Represents a three-dimensional vector More... | |
struct | Matrix3x3 |
Represents a 3 x 3 matrix More... | |
struct | Point2d |
Represents two-dimensional cartesian coordinates for a point More... | |
struct | Point4d |
Represents four-dimensional homogeneous coordinates for a point. More... | |
class | UI |
This class contains the various elements that represent the NX User Interface. More... | |
class | Unit |
Represents a unit More... | |
class | UnitCollection |
Provides methods for manipulating the units in a part More... | |
class | Update |
Provides methods for update and delete. More... | |
class | Validation |
Represents an NX NXOpen.Validation object. More... | |
class | ValidationCollection |
Represents a collection of NXOpen.Validation . More... | |
class | View |
Represents a view. More... | |
class | ViewCollection |
Represents a collection of NXOpen.View s. More... | |
class | ViewDependentDisplayManager |
Represents all view dependent display operations More... | |
class | ViewUIManager |
More... | |
class | VirtuallabImporter |
Represents a VirtuallabImporter to be used when importing the Virtuallab Data This class is created using DexManager . More... | |
class | VRMLImporter |
Used to import a VRML file into the work part. More... | |
class | WCS |
Represents the World Coordinate System. More... | |
class | WidthDefinition |
Represents a NXOpen.WidthDefinition , which is a representation of an NX width palette. More... | |
class | Xform |
Represents a smart xform More... | |
class | XformCollection |
Represents a collection of NXOpen.Xform objects. More... | |
Enumerations | |
enum | LightType { Ambient, Distant, Eye, Point, Spot, Scene = 6 } |
The type of a light. More... | |
enum | ExtrudeLimitDataLimitType { Distance, UntilNext, UntilSelected, UntilSelectedExtendFace, ThroughAll } |
This enum represents the type of limit More... | |
enum | ExtrudeOffsetDataOffsetType { None, NormalOffset, SymmetricOffset, SingleOffset } |
This enum represents the type of offset More... | |
enum | ExtrudeTaperDataTaperType { None, SimpleFromStart, SimpleFromProfile, Symmetric, MatchedEnds, Asymmetric } |
This enum represents the type of taper More... | |
enum | FileNewApplication { Drafting, Modeling, Studio, Assemblies, Gateway, RoutingElectrical, RoutingMechanical, RoutingLogical, Nxsheetmetal, SheetTemplate, CaeFem, CaeSim, AeroSheetmetal, FlexPcdSheetmetal, CaeAssyFem, Cam, Inspection, Mechatronics, ShipContainer, ShipDetail, ShipReference, ShipSystem, Welding, WeldingJoint, Nxle, ShipGaAssembly, ShipGaSystem, Last } |
The application type of the new file being created through a template More... | |
enum | FileNewTemplateType { Workset, Item, DesignElement, DesignControlElement, DesignFeature, Generic, Sheet, DiagrammingSheetpart, Last } |
Enumeration used for templates to determine the type of the template. More... | |
enum | LineWidthOption { Assigned, Default, NoChange } |
the line width options. More... | |
enum | DisplayPartOption { ReplaceExisting, AllowAdditional } |
Controls whether or not a new display part may be displayed in addition to existing display parts, or instead of the currently active display part. More... | |
enum | PartDisplayPartWorkPartOption { SameAsDisplay, UseLast } |
Controls what the work part will be when setting active display part. More... | |
enum | ScEvaluationFiltertype { SleepyEntity = 1 } |
Tokens used to create different evaluation filters on ScCollector More... | |
enum | FollowFilletRuleType { Connected, Tangent } |
Selection Intent method to use with follow fillet rule. More... | |
enum | ApparentChainingRuleType { Connected, Tangent, Dumb } |
Selection Intent method to use with apparent chaining. More... | |
enum | ApparentChainingRuleSelection { AllowAllTypes, AllowCurve, AllowEdge } |
Selection Intent filter method to use with apparent chaining. More... | |
enum | AxisOrientation { Horizontal, Vertical } |
Specifies axis orientation More... | |
enum | Sense { Forward, Reverse } |
Specifies sense direction More... | |
enum | PlaneNormalOrientation { Inward, Outward } |
Specifies the orientation of a plane's normal More... | |
enum | RotationDirection { RightHand, LeftHand } |
Specifies rotation direction More... | |
enum | Persistence { Temporary, Permanent } |
Specifies persistence More... | |
enum | CurveParameterType { ArcLength, PercentArcLength, ThroughPoint } |
Specifies curve parameter type as arc length or percent arc length More... | |
enum | XYZAxis { XAxis, YAxis, ZAxis } |
Specifies the X, Y, or Z axis More... | |
enum | OriginMethod { SpecifyPoint, WorkPartOrigin } |
Specifies origin method More... | |
Provides classes and interfaces for the NX Open Common API.
Controls whether or not a new display part may be displayed in addition to existing display parts, or instead of the currently active display part.
See NXOpen.PartCollection.SetActiveDisplay
Enumerator | |
---|---|
ReplaceExisting |
Replace the existing active display part with the new one |
AllowAdditional |
If possible display the new part as an additional display part |
The application type of the new file being created through a template
Enumeration used for templates to determine the type of the template.
enum NXOpen.LightType |
The type of a light.
For now, you can only modify lights of type LightType.Scene via automation languages.
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return a null reference (Nothing in Visual Basic).
the line width options.
This is used in conjunction with NXOpen.LineWidthBuilder
Enumerator | |
---|---|
Assigned |
Width value can be obtained from the builder. For example, NXOpen.LineWidthBuilder.Width |
Default |
Default width. The builder interprets this option as per its need. |
NoChange |
Do not modify the width. |
enum NXOpen.OriginMethod |
Controls what the work part will be when setting active display part.
See NXOpen.PartCollection.SetActiveDisplay
Enumerator | |
---|---|
SameAsDisplay |
New work part will be set to the new display part |
UseLast |
If possible use the work part that was used when this part was last the display part |
enum NXOpen.Persistence |
enum NXOpen.Sense |
enum NXOpen.XYZAxis |