System Control Overview | Statement List
The LAYC statement defines any of the standard NX layouts. You can create a single view, a two view (side by side), a two view (top and bottom), a four view, or a six view layout. The views in the layout are specified by their view name. All view names specified must be existing views.
The LAYC command is not available in the Drafting application.
An LAYC layout can become the current, active layout as it is being created, or the layout can be created without having any effect on the current display. If the layout becomes the active layout, the view can be retrieved at its last saved scale, to a specified scale, or by using an Fit operation.