Sheet Body Overview | Statement List
CONE creates a sheet body whose underlying surface type is a cone. Cones are analytical surfaces. The basic elements required to create a cone are: a vertex, a vertex angle and/or a radius, and a vector defining the vertex direction.
When a vertex angle is specified, the value is equal to half the included angle of the vertex. The angle is measured from the axis of the cone to the cone side.