&ANGTOL
Sets/reads the angle tolerance used in the Modeling Application for many curve and sheet body creation and editing operations.
Statements that specify an angle tolerance using the optional minor word TOLER will override the angle tolerance value set interactively in NX using the Preferences->Modeling option. If one of these statements doesn't specify the optional angle tolerance value, the system uses the angle tolerance value set in the NX option.
Read/Write - Number - Greater Than Zero