File Management Overview | Statement List
This section covers the GRIP BATCH statements, which can be used to compile, link, execute, and/or cancel GRIP programs in an unattended mode.
If the following major words are present in a program which is executing in batch mode, they will be ignored:
MESSG
LSTDEV
RPAINT
If the following major words are present in a program, the execution module will be flagged as interactive which will deny batch processing:
CHOOSE
GPOS
IDENT
IDSCH
PARAM
POS
TEXT