GRIP errors divide into the following categories:
Error Range |
Error Type |
1-99 |
Non-fatal compilation errors. Compilation continues but object code cannot be filed. |
100-199 |
Fatal compilation errors. Compilation is halted. |
500-599* |
Compiler system errors. |
600-699* |
Interpreter system errors. |
1545000- |
Non-fatal execution errors. Program execution may be continued. |
1549000- |
Fatal execution errors. Program execution is halted. |
Errors numbered 500-699 indicate a malfunction in NX and should be reported to the Global Technical Access Center (GTAC). The GTAC toll-free telephone number is: 1-800-955-0000.