Automating Program Development with Scripts
You can automate GRIP program development using batch files. With the appropriate switches and arguments you can compile, link, or execute a GRIP program. For Windows platforms, we supply MS-DOS batch files.
The batch files are located at "UGII_BASE_DIR/ugii/gripbatch". The batch files start the GCAL and the NX image. The GCAL image is located at "UGII_BASE_DIR\ugopen\gcal". With the provided information, you can also customize and develop your own batch files. You can use the "gripbatch" files in two ways: Compile and Link or Execute a GRIP Program. The syntax for both tasks is listed below.
One use of the gripbatch batch file is to compile and/or link GRIP programs using the GCAL image, which is located at "UGII_BASE_DIR/ugopen/gcal".
gripbatch {[-compile] [-link]}
[-erlst]
[-device:<listing_device>]
[-name:<output_file_name>]
[-dir:<directory_name>]
[-list]
filespec
Another use of the gripbatch batch file is to execute GRIP programs using the NX image.
gripbatch -r
[-device:<listing_device>]
[-name:<output_file_name>]
[-dir:<directory_name>]
filespec
["string"]
Any item with a "-" in front of it, is a switch. Switches must follow the command and are not order dependent. Items without a "-" in front are arguments to the command. Arguments must be given in the order indicated above.
Arguments in [] brackets are optional, do not type the [] brackets. At least one of the arguments enclosed in {} brackets must be specified, do not type {} brackets.