UF_PD_allowable_geometry_e (view source)
Defined in: uf_pd_types.h
Overview
Following is the enumerated type used to define the set of valid
geometry types for a product definition attribute.
Data Members
UF_PD_ALLOWABLE_GEOMETRY_ALL
UF_PD_ALLOWABLE_GEOMETRY_EDGE
UF_PD_ALLOWABLE_GEOMETRY_FACE
UF_PD_ALLOWABLE_GEOMETRY_BODY
UF_PD_ALLOWABLE_GEOMETRY_LINE
UF_PD_ALLOWABLE_GEOMETRY_POINT
UF_PD_ALLOWABLE_GEOMETRY_CONIC
UF_PD_ALLOWABLE_GEOMETRY_ARC
UF_PD_ALLOWABLE_GEOMETRY_SPLINE
UF_PD_ALLOWABLE_GEOMETRY_COMPONENT
UF_PD_attribute_type_e (view source)
Defined in: uf_pd_types.h
Also known as:
Overview
This enumerated type defines the type of attributes
current supported by the Smart Model tools.
Data Members
UF_PD_NULL_ATTRIBUTE_TYPE
UF_PD_UG_USER_DEFINED
UF_PD_STRING_TYPE
UF_PD_INTEGER_TYPE
UF_PD_NUMBER_TYPE
UF_PD_ENTERPRISE_IDENTIFIER_TYPE
UF_PD_PART_IDENTIFIER_TYPE
UF_PD_MATERIAL_SPECIFICATION_TYPE
UF_PD_PROCESS_SPECIFICATION_TYPE
UF_PD_SURFACE_FINISH_TYPE
UF_PD_GENERIC_NOTE_TYPE
UF_PD_SPECIFIC_NOTE_TYPE
UF_PD_BALLOON_NOTE_TYPE
UF_PD_LOCATOR_DESIGNATOR_TYPE
UF_PD_COORDINATE_NOTE_TYPE
UF_PD_EXPORT_CONTROL_TYPE
UF_PD_GOVERNMENT_SECURITY_INFO_TYPE
UF_PD_COMPANY_PROPRIETARY_INFO_TYPE
UF_PD_GENERIC_EMARKING_TYPE
UF_PD_SPUR_GEAR_TYPE
UF_PD_HELICAL_GEAR_TYPE
UF_PD_STRAIGHT_SIDED_SPLINE_TYPE
UF_PD_INVOLUTE_SPLINE_TYPE
UF_PD_NUM_ATTRIBUTE_TYPES
UF_PD_attribute_value_type_e (view source)
Defined in: uf_pd_types.h
Also known as:
- UF_PD_attribute_value_type_t
Overview
This enumerated type defines the type of attribute values
available.
Data Members
UF_PD_INTEGER_VALUE
UF_PD_NUMBER_VALUE
UF_PD_STRING_VALUE
UF_PD_LIST_VALUE
UF_PD_URL_VALUE
UF_PD_BUS_MODFR_type_e (view source)
Defined in: uf_pd_types.h
Overview
Following is the enumerated type used to define the set of valid
business modifier types for a product definition attribute.
Data Members
UF_PD_BUS_MODFR_STRING_TYPE = 0
UF_PD_BUS_MODFR_LIST_TYPE
UF_PD_BUS_MODFR_URL_TYPE
UF_PD_BUS_MODFR_REVISION_TYPE
UF_PD_BUS_MODFR_SAFETY_CLASS_TYPE
UF_PD_BUS_MODFR_CUSTOMER_VALUE_TYPE
UF_PD_product_definition_instance_type_e (view source)
Defined in: uf_pd_types.h
Also known as:
- UF_PD_product_definition_instance_type_t
Overview
Defines the type of user defined instance object
Data Members
UF_PD_PRODUCT_DEFINITION_INSTANCE_COMBINED
UF_PD_PRODUCT_DEFINITION_INSTANCE_USER_DEFINED
UF_PD_product_definition_leader_assoc_pnt_type_e (view source)
Defined in: uf_pd_types.h
Also known as:
- UF_PD_product_definition_leader_assoc_pnt_type_t
Overview
The following structure is used to defined instance leader
associated point information
Data Members
UF_PD_INSTANCE_LEADER_ASSOC_PNT_TAG_TYPE
UF_PD_INSTANCE_LEADER_ASSOC_NOMINAL_TYPE