/*
uf_obj_types.h
*******************************************************************************/
#ifndef UF_OBJ_TYPES_INCLUDED
#define UF_OBJ_TYPES_INCLUDED
#include <uf_defs.h>
#define UF_OBJ_DELETED 0
#define UF_OBJ_TEMPORARY 1
#define UF_OBJ_CONDEMNED 2
#define UF_OBJ_ALIVE 3
/* For use with UF_VIEW_ask/set_visualization*/
#define UF_OBJ_COLOR_ORIGINAL (-1)
#define UF_OBJ_FONT_ORIGINAL (-1)
/*
UF_OBJ_<COLOR> symbols should no longer be used.
Symbols such as UF_OBJ_BLUE define color indices. In releases
prior to NX3, each defined index referenced the indicated color
in the default color definition file (CDF) provided with NX. For
example, the default CDF assigned blue to color index UF_OBJ_BLUE
(1), green to color index UF_OBJ_GREEN (2), etc.
Beginning with NX3, the default CDF does not assign these colors
to these indices. The default CDF assigns pale/light colors to
color indices 1 through 15 instead of the familiar legacy colors
(green, blue, cyan, etc.). Using UF_OBJ_<COLOR> symbols with the
default CDF will not produce the expected color.
Instead of using UF_OBJ_<COLOR> symbols, call one of the following
functions to obtain the color index that references the desired
color.
UF_DISP_ask_closest_color
UF_DISP_ask_closest_color_in_part
UF_DISP_ask_closest_color_in_displayed part
*/
#define UF_OBJ_LEGACY_BLUE 1
#define UF_OBJ_LEGACY_GREEN 2
#define UF_OBJ_LEGACY_CYAN 3
#define UF_OBJ_LEGACY_RED 4
#define UF_OBJ_LEGACY_MAGENTA 5
#define UF_OBJ_LEGACY_YELLOW 6
#define UF_OBJ_LEGACY_WHITE 7
#define UF_OBJ_LEGACY_OLIVE 8
#define UF_OBJ_LEGACY_PINK 9
#define UF_OBJ_LEGACY_BROWN 10
#define UF_OBJ_LEGACY_ORANGE 11
#define UF_OBJ_LEGACY_PURPLE 12
#define UF_OBJ_LEGACY_DARK_RED 13
#define UF_OBJ_LEGACY_AQUAMARINE 14
#define UF_OBJ_LEGACY_GRAY 15
#define UF_OBJ_BLUE UF_OBJ_LEGACY_BLUE
#define UF_OBJ_GREEN UF_OBJ_LEGACY_GREEN
#define UF_OBJ_CYAN UF_OBJ_LEGACY_CYAN
#define UF_OBJ_RED UF_OBJ_LEGACY_RED
#define UF_OBJ_MAGENTA UF_OBJ_LEGACY_MAGENTA
#define UF_OBJ_YELLOW UF_OBJ_LEGACY_YELLOW
#define UF_OBJ_WHITE UF_OBJ_LEGACY_WHITE
#define UF_OBJ_OLIVE UF_OBJ_LEGACY_OLIVE
#define UF_OBJ_PINK UF_OBJ_LEGACY_PINK
#define UF_OBJ_BROWN UF_OBJ_LEGACY_BROWN
#define UF_OBJ_ORANGE UF_OBJ_LEGACY_ORANGE
#define UF_OBJ_PURPLE UF_OBJ_LEGACY_PURPLE
#define UF_OBJ_DARK_RED UF_OBJ_LEGACY_DARK_RED
#define UF_OBJ_AQUAMARINE UF_OBJ_LEGACY_AQUAMARINE
#define UF_OBJ_GRAY UF_OBJ_LEGACY_GRAY
#define UF_OBJ_MIN_COLOR 1
#define UF_OBJ_MAX_COLOR 216
/* For use with UF_OBJ_ask_display_properties/UF_OBJ_set_blank_status */
#define UF_OBJ_NOT_BLANKED 0
#define UF_OBJ_BLANKED 1
/* For use with UF_OBJ_ask_display_properties/UF_OBJ_set_line_width */
#define UF_OBJ_WIDTH_ORIGINAL (-1)
#define UF_OBJ_WIDTH_NORMAL 0
#define UF_OBJ_WIDTH_THICK 1
#define UF_OBJ_WIDTH_THIN 2
/* Support new line width types*/
#define UF_MIN_NEW_WIDTH 5
#define UF_OBJ_WIDTH_1 (UF_MIN_NEW_WIDTH + 0)
#define UF_OBJ_WIDTH_2 (UF_MIN_NEW_WIDTH + 1)
#define UF_OBJ_WIDTH_3 (UF_MIN_NEW_WIDTH + 2)
#define UF_OBJ_WIDTH_4 (UF_MIN_NEW_WIDTH + 3)
#define UF_OBJ_WIDTH_5 (UF_MIN_NEW_WIDTH + 4)
#define UF_OBJ_WIDTH_6 (UF_MIN_NEW_WIDTH + 5)
#define UF_OBJ_WIDTH_7 (UF_MIN_NEW_WIDTH + 6)
#define UF_OBJ_WIDTH_8 (UF_MIN_NEW_WIDTH + 7)
#define UF_OBJ_WIDTH_9 (UF_MIN_NEW_WIDTH + 8)
#define UF_OBJ_MAX_WIDTH (UF_OBJ_WIDTH_9 + 1)
#define UF_OBJ_is_valid_width( width ) \
( (((width) >= (int)UF_OBJ_WIDTH_NORMAL) && ((width) <= (int)UF_OBJ_WIDTH_THIN)) || \
(((width) >= (int)UF_MIN_NEW_WIDTH) && ((width) < (int)UF_OBJ_MAX_WIDTH)) )
/*
UF_OBJ_is_valid_inherited_width is used to validate line width for an object
that can inherit its line width value from another object. In this case,
line width value of the object is represented by UF_OBJ_WIDTH_ORIGINAL.
Note that UF_OBJ_WIDTH_ORIGINAL is not a valid setting for all objects.
*/
#define UF_OBJ_is_valid_inherited_width( width ) \
( ((width) == UF_OBJ_WIDTH_ORIGINAL) || UF_OBJ_is_valid_width(width) )
/*
*/
#define UF_OBJ_NAME_NCHARS 128
#define UF_OBJ_NAME_BUFSIZE NX_BUFSIZE(UF_OBJ_NAME_NCHARS)
/*
UF_OBJ_NAME_LEN is being deprecated because NX is moving to support
multibyte characters. User written programs should start using the
new definitions above for object names:
UF_OBJ_NAME_BUFSIZE should be used for buffer allocations and memory
allocations, e.g. char my_obj_name[UF_OBJ_NAME_BUFSIZE]
UF_OBJ_NAME_NCHARS should be used to limit the number of characters in
a buffer. NX code will enforce these limits.
New routines have been added which will help in this transition:
UF_TEXT_count_characters() will count the number of characters in a string.
UF_TEXT_truncate() will terminate a C string such that it will fit in a
buffer of a given size and not exceed a character count.
MAX_INFO_NAME_LEN is being deprecated as it is unused. User written programs
should be changed to no longer use this definition.
*/
/* */
#define UF_OBJ_NAME_LEN (UF_OBJ_NAME_BUFSIZE-1)
#define MAX_INFO_NAME_LEN (UF_OBJ_NAME_BUFSIZE*3)
/* */
/* For use with UF_OBJ_ask_display_properties/UF_OBJ_cycle_by_name */
#define UF_OBJ_OK 0
#define UF_OBJ_NAME_NOT_FOUND 1
/* For use with view dependent edits */
#define UF_OBJ_FONT_INVISIBLE 0
#define UF_OBJ_FONT_SOLID 1
#define UF_OBJ_FONT_DASHED 2
#define UF_OBJ_FONT_PHANTOM 3
#define UF_OBJ_FONT_CENTERLINE 4
#define UF_OBJ_FONT_DOTTED 5
#define UF_OBJ_FONT_LONG_DASHED 6
#define UF_OBJ_FONT_DOTTED_DASHED 7
/* special object types */
#define UF_OBJ_EXPR_TYPE 65536
#define UF_OBJ_PART_TYPE 65537
/* Display properties of the object */
struct UF_OBJ_disp_props_s {
int layer; /* the layer an object resides on */
int color; /* the color an object possesses */
int blank_status; /* the blank status of an object
This status is defined by one of
the two string defined constants:
UF_OBJ_NOT_BLANKED
UF_OBJ_BLANKED
*/
int line_width; /* the line width of an object
Can be one of the following :
UF_OBJ_WIDTH_NORMAL
UF_OBJ_WIDTH_THICK
UF_OBJ_WIDTH_THIN
UF_OBJ_WIDTH_ORIGINAL
UF_OBJ_WIDTH_1 -- UF_OBJ_WIDTH_9
*/
int font; /* the font an object possesses */
logical highlight_status; /* the highlight status of an object
where TRUE indicates that highlight
is on.
*/
};
typedef struct UF_OBJ_disp_props_s UF_OBJ_disp_props_t,
*UF_OBJ_disp_props_p_t;
/******************************************************************************
*
* Color, Line Font and Width Settings
*
*****************************************************************************/
/* Structure used by UF_OBJ_ask_cre_settings and UF_OBJ_ask_def_cre_settings
* to return color/line font/width settings
* Please refer to the constants and numerical values
* for string defined constants or numerical values to be used for each one of
* the fields in this structure
*/
struct UF_OBJ_cre_settings_s {
int color;
int line_font;
int width;
};
typedef struct UF_OBJ_cre_settings_s UF_OBJ_cre_settings_t,
*UF_OBJ_cre_settings_p_t;
/* Type/Subtype Property Definitions
*
* No Type/Subtype Properties
*/
#define UF_OBJ_no_property (0)
/* UF_solid_type Properties
*/
#define UF_OBJ_solid_body_property (1)
#define UF_OBJ_sheet_body_property (2)
/* Translucency is an integer value in the range of
* 0 (no translucency) to 100 (fully translucent). It
* applies only to object types which may be shaded, such
* as solid/sheet bodies, solid/sheet faces, and
* faceted representations.
*/
typedef int UF_OBJ_translucency_t, *UF_OBJ_translucency_p_t;
#endif /* UF_OBJ_TYPES_INCLUDED */