/*
uf_modl_pockets.h
File description:
Open API modeling routines to create, edit and inquire about pockets.
*****************************************************************************/
#ifndef UF_MODL_POCKETS_H_INCLUDED
#define UF_MODL_POCKETS_H_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_modl_types.h>
#include <libufun_exports.h>
/********************************************************************
Gets rectangular pocket parameters.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_rect_pocket_parms(
tag_t feature_obj_id ,/* <I>
A feature object identifier
*/
int edit ,/* <I>
This is an unused flag. It used to determine whether
to return the right-hand side or both sides of an
expression. Currently, both sides of an expression
are returned.
*/
char * length[3],/* <OF>
Pointer to an array of three character pointers for
length, width, and depth. This must be freed by
calling UF_free.
*/
char ** corner_rad ,/* <OF>
Pocket corner radius. This must be freed by
calling UF_free.
*/
char ** floor_rad ,/* <OF>
Pocket floor radius. This must be freed by
calling UF_free.
*/
char ** taper_angle /* <OF>
Pocket taper angle. This must be freed by
calling UF_free.
*/
);
/********************************************************************
Gets cylinder pocket parameters.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_cyl_pocket_parms(
tag_t feature_obj_id ,/* <I>
A feature object identifier
*/
int edit ,/* <I>
This is an unused flag. It used to determine whether
to return the right-hand side or both sides of an
expression. Currently, both sides of an expression
are returned.
*/
char ** diameter ,/* <OF>
Cylinder diameter. This must be freed by
calling UF_free.
*/
char ** depth ,/* <OF>
Cylinder depth. This must be freed by
calling UF_free.
*/
char ** floor_rad ,/* <OF>
Floor radius. This must be freed by
calling UF_free.
*/
char ** taper_angle /* <OF>
Taper angle. This must be freed by
calling UF_free.
*/
);
/****************************************************************************
Creates a cylindrical pocket feature using a location, direction,
diameter, depth, floor radius, and taper angle. Along with these items
a placement face is needed to determine which face the pocket is
associated to. The output of this function is the object identifier
associated to the cylindrical pocket.
Environment: Internal and External
See Also:
History:
***************************************************************************/
extern UFUNEXPORT int UF_MODL_create_cyl_pocket(
double location[3] ,/* <I>
Cylindrical pockets location.
*/
double direction[3] ,/* <I>
Cylindrical pockets direction.
*/
char * diame ,/* <I>
Cylindrical pockets diameter.
*/
char * depth ,/* <I>
Cylindrical pockets depth.
*/
char * radius ,/* <I>
Cylindrical pockets floor radius.
*/
char * angle ,/* <I>
Cylindrical pockets taper angle.
*/
tag_t face ,/* <I>
Face for the RPO constraint.
*/
tag_t * feature_obj_id /* <O>
Feature object identifier of created pocket
*/
);
/****************************************************************************
Creates a rectangular pocket feature using the location, direction, X
direction, size, corner radius, floor radius and taper angle. Along with
these items a placement face is needed to determine which face the
pocket is associated to. The output of this function is the object
identifier associated to the rectangular pocket.
Return:
Return code:
= 0: successful
> 0: failing error number
< 0: failing error number
Environment: Internal and External
History: For V18.0, a datum plane may be input as the face defining the
RPO constraint.
See Also: See example
UF_MODL_ask_rect_pocket_parms
***************************************************************************/
extern UFUNEXPORT int UF_MODL_create_rect_pocket(
double location[3] ,/* <I>
Rectangular pocket location.
*/
double direction[3] ,/* <I>
Rectangular pocket direction.
*/
double x_dir[3] ,/* <I>
Rectangular pocket x direction.
*/
char * len[3] ,/* <I>
Rectangular pocket size.
*/
char * corner ,/* <I>
Rectangular pocket corner radius.
*/
char * floor ,/* <I>
Rectangular pocket floor radius.
*/
char * angle ,/* <I>
Rectangular pocket taper angle.
*/
tag_t face ,/* <I>
Face for the RPO constraint (may be a datum plane).
*/
tag_t * feature_obj_id /* <O>
Feature object identifier of created rect. pocket
*/
);
/******************************************************************************
Creates a general pocket. Creates Expressions for the taper_angle,
floor_offset, placement_radius, and floor_radius if they are used.
Environment: Internal and External
See Also:
UF_MODL_ask_general_pocket
UF_MODL_edit_general_pocket
UF_MODL_free_general_pocket
please see example
History:
******************************************************************************/
extern UFUNEXPORT int UF_MODL_create_general_pocket(
UF_MODL_faces_p_t placement_faces ,/* <I>
The faces or a face collector used to define the shape of
the pocket at the placement faces. The
first face is used to determine the
target body.
*/
UF_MODL_offset_trans_faces_p_t floor_faces ,/* <I>
The faces or a face collector used to define
the floor of the pocket. The floor can either be an
offset or translation of the
specified faces. If it is desired
to have the floor be an offset
or translate of the
placement faces, then just set the
UF_MODL_faces_p_t pointer within
this input structure to the
placement_faces pointer value.
*/
UF_MODL_pocketpad_outline_p_t outline ,/* <I>
The definition of the curves used to
define the shape of the pocket.
The shape can be defined by a single set of
curves or section builder at either the placement face or
the floor face, and then the other
curves or section builder are derived with a taper angle.
The shape can also be defined by
specifying curves or section builders at both the
placement face and the floor face.
*/
UF_MODL_parm_p_t placement_radius ,/* <I>
The specification of the radius desired
between the side of the pocket and the
placement face.
*/
UF_MODL_parm_p_t floor_radius ,/* <I>
The specification of the radius desired
between the side of the pocket and the
floor of the pocket.
*/
tag_t * general_pocket_tag /* <O>
Object identifier for the general
pocket feature.
*/
);
/******************************************************************************
Retrieves the parameters used to create a general pocket.
Environment: Internal and External
See Also:
UF_MODL_create_general_pocket
UF_MODL_edit_general_pocket
UF_MODL_free_general_pocket
Refer to example
History:
******************************************************************************/
extern UFUNEXPORT int UF_MODL_ask_general_pocket(
tag_t general_pocket_tag ,/* <I>
Object identifier of the general pocket
feature whose parameters are to be
retrieved.
*/
UF_MODL_faces_p_t placement_faces ,/* <OF>
The faces used to define the shape of the
pocket at the placement faces. The first face
is used to determine the target body. The
caller must allocate a UF_MODL_faces_t
structure, and pass in a pointer to that
structure. The structure will be filled
with allocated data which can be freed by
calling UF_MODL_free_general_pocket.
*/
UF_MODL_offset_trans_faces_p_t floor_faces ,/* <OF>
The definition of the floor of the pocket.
The floor can either be an offset or
translation of the specified faces. If the
floor was an offset or translate of the
placement faces, then the UF_MODL_faces_p_t
pointer within this structure, points to the
placement faces structure. The caller must
allocate a UF_MODL_offset_trans_faces_t
structure, and pass in a pointer to that
structure. The structure will be filled
with allocated data which can be freed by
calling UF_MODL_free_general_pocket.
*/
UF_MODL_pocketpad_outline_p_t outline ,/* <OF>
The definition of the curves used to
define the shape of the pocket. The
shape can be defined by a single set of
curves at either the placement face or
the floor face, and then the other
curves are derived with a taper angle.
The shape can also be defined by specifying
curves at both the placement face and the
floor face. The caller must allocate a
UF_MODL_pocketpad_outline_t structure, and
pass in a pointer to that structure. The
structure will be filled with allocated
data which can be freed by calling
UF_MODL_free_general_pocket.
*/
UF_MODL_parm_p_t placement_radius ,/* <OF>
The specification of the radius desired
between the side of the pocket and the
placement face. The caller must allocate a
UF_MODL_parm_p_t structure, and
pass in a pointer to that structure. The
structure will be filled with allocated
data which can be freed by calling
UF_MODL_free_general_pocket.
*/
UF_MODL_parm_p_t floor_radius /* <OF>
The specification of the radius desired
between the side of the pocket and the
floor of the pocket. The caller must allocate a
UF_MODL_parm_p_t structure, and
pass in a pointer to that structure. The
structure will be filled with allocated
data which can be freed by calling
UF_MODL_free_general_pocket.
*/
);
/******************************************************************************
Retrieves the parameters with face collectors and section builders
used to create a general pocket.
Environment: Internal and External
See Also:
UF_MODL_create_general_pocket
UF_MODL_edit_general_pocket
UF_MODL_free_general_pocket
Refer to example
History:
******************************************************************************/
extern UFUNEXPORT int UF_MODL_ask_general_pocket1(
tag_t general_pocket_tag ,/* <I>
Object identifier of the general pocket
feature whose parameters are to be
retrieved.
*/
UF_MODL_faces_p_t placement_faces ,/* <OF>
The face collector used to define the shape of the
pocket at the placement faces. The first face
of the collector is used to determine the target body. The
caller must allocate a UF_MODL_faces_t
structure, and pass in a pointer to that
structure. The structure will be filled
with allocated data which can be freed by
calling UF_MODL_free_general_pocket.
*/
UF_MODL_offset_trans_faces_p_t floor_faces ,/* <OF>
The definition of the floor of the pocket.
The floor can either be an offset or
translation of the specified face collector. If the
floor was an offset or translate of the
placement faces, then the UF_MODL_faces_p_t
pointer within this structure, points to the
placement faces structure. The caller must
allocate a UF_MODL_offset_trans_faces_t
structure, and pass in a pointer to that
structure. The structure will be filled
with allocated data which can be freed by
calling UF_MODL_free_general_pocket.
*/
UF_MODL_pocketpad_outline_p_t outline ,/* <OF>
The definition of the curves used to
define the shape of the pocket. The
shape can be defined by a single section builder
at either the placement face or
the floor face, and then the other
section builder is derived with a taper angle.
The shape can also be defined by specifying
section builders at both the placement face and the
floor face. The caller must allocate a
UF_MODL_pocketpad_outline_t structure, and
pass in a pointer to that structure. The
structure will be filled with allocated
data which can be freed by calling
UF_MODL_free_general_pocket.
*/
UF_MODL_parm_p_t placement_radius ,/* <OF>
The specification of the radius desired
between the side of the pocket and the
placement face. The caller must allocate a
UF_MODL_parm_p_t structure, and
pass in a pointer to that structure. The
structure will be filled with allocated
data which can be freed by calling
UF_MODL_free_general_pocket.
*/
UF_MODL_parm_p_t floor_radius /* <OF>
The specification of the radius desired
between the side of the pocket and the
floor of the pocket. The caller must allocate a
UF_MODL_parm_p_t structure, and
pass in a pointer to that structure. The
structure will be filled with allocated
data which can be freed by calling
UF_MODL_free_general_pocket.
*/
);
/******************************************************************************
Edits the various parameters of the general pocket and reconstructs it
based on these new parameters.
Environment: Internal and External
See Also: Refer to example
UF_MODL_ask_general_pocket
UF_MODL_create_general_pocket
UF_MODL_free_general_pocket
History:
****************************************************************************/
extern UFUNEXPORT int UF_MODL_edit_general_pocket(
tag_t general_pocket_tag ,/* <I>
Object identifier of the general pocket
feature to be modified.
*/
UF_MODL_faces_p_t placement_faces ,/* <I>
The faces or collector of faces used to define the shape of
the pocket at the placement faces. The
first face is used to determine the target
body.
*/
UF_MODL_offset_trans_faces_p_t floor_faces ,/* <I>
The faces or face collectors used to define
the floor of the pocket. The floor can
either be an offset or
translation of the specified
faces or face collector. If it is desired to have
the floor be an offset or
translate of the placement
faces, then just set the
UF_MODL_faces_p_t
pointer within this input
structure to the placement_faces
pointer value.
*/
UF_MODL_pocketpad_outline_p_t outline ,/* <I>
The definition of the curves used to
define the shape of the pocket. The
shape can be defined by a single set of
curves or section builder at either the placement face or
the floor face, and then the other curves or section builder
are derived with a taper angle. The
shape can also be defined by specifying
curves or section builder at both the placement face and
the floor face.
*/
UF_MODL_parm_p_t placement_radius ,/* <I>
The specification of the radius desired
between the side of the pocket and the
placement face.
*/
UF_MODL_parm_p_t floor_radius /* <I>
The specification of the radius desired
between the side of the pocket and the
floor of the pocket.
*/
);
/******************************************************************************
Frees all the memory associated with the parameters returned from
UF_MODL_ask_general_pocket. Refer to the description of
UF_MODL_create_general_pocket for an example of how to use this function.
Environment: Internal and External
See Also:
UF_MODL_ask_general_pocket
UF_MODL_create_general_pocket
UF_MODL_edit_general_pocket
History:
******************************************************************************/
extern UFUNEXPORT int UF_MODL_free_general_pocket(
UF_MODL_faces_p_t placement_faces ,/* <I>
The faces used to define the shape of
the pocket at the placement faces. The
first face is used to determine the
target body.
*/
UF_MODL_offset_trans_faces_p_t floor_faces ,/* <I>
The definition of the floor of
the pocket. The floor can either
be an offset or translation of
the specified faces. If it is
desired to have the floor
be an offset or translate of the
placement faces, then just set i
the UF_MODL_faces_p_t pointer
within this input structure to
the placement_faces pointer
value.
*/
UF_MODL_pocketpad_outline_p_t outline ,/* <I>
The definition of the curves used to
define the shape of the pocket. The
shape can be defined by a single set of
curves at either the placement face or
the floor face, and then the other
curves are derived with a taper angle.
The shape can also be defined by
specifying curves at both the
placement face and the floor face.
*/
UF_MODL_parm_p_t placement_radius ,/* <I>
The specification of the radius desired
between the side of the pocket and the
placement face.
*/
UF_MODL_parm_p_t floor_radius /* <I>
The specification of the radius desired
between the side of the pocket and the
floor of the pocket.
*/
);
#undef EXPORTLIBRARY
#endif /* UF_MODL_POCKETS_H_INCLUDED */