/*
uf_modl_grooves.h
File description:
Open API modeling routines to create, edit and inquire about grooves.
*****************************************************************************/
#ifndef UF_MODL_GROOVES_H_INCLUDED
#define UF_MODL_GROOVES_H_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_modl_types.h>
#include <libufun_exports.h>
/********************************************************************
Creates a ball groove feature by inputting its location, direction,
diameter and width. Along with these items a placement face is
needed to determine which face the ball groove is associated to. The
output of this function is the object identifier associated to the ball
groove.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_create_ball_groove(
double location[3] ,/* <I>
Ball groove location.
*/
double direction[3] ,/* <I>
Ball groove direction
*/
char * diame ,/* <I>
Ball groove diameter.
*/
char * width ,/* <I>
Ball groove width.
*/
tag_t face ,/* <I>
Face for the RPO constraint.
*/
tag_t * feature_obj_id /* <O>
Feature object identifier of created ball groove
*/
);
/********************************************************************
Gets U groove parameters.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_u_groove_parms(
tag_t feature_obj_id ,/* <I>
A feature object identifier.
*/
int edit ,/* <I>
This is an unused flag. It was used to determine
whether to return the right-hand side or both sides
of an expression. Currently, both sides of an
expression are returned.
*/
char ** groove_dia ,/* <OF>
Groove diameter. This must be freed by
calling UF_free.
*/
char ** width ,/* <OF>
Groove width. This must be freed by
calling UF_free.
*/
char ** corner_rad /* <OF>
Groove corner radius. This must be freed by
calling UF_free.
*/
);
/********************************************************************
Gets rectangular groove parameters.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_rect_groove_parms(
tag_t feature_obj_id ,/* <I>
A feature object identifier
*/
int edit ,/* <I>
This is an unused flag. It was used to determine
whether to return the right-hand side or both sides
of an expression. Currently, both sides of an
expression are returned.
*/
char **groove_dia ,/* <OF>
Groove diameter. This must be freed by
calling UF_free.
*/
char **width /* <OF>
Groove width. This must be freed by
calling UF_free.
*/
);
/********************************************************************
Gets ball groove parameters.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_ball_groove_parms(
tag_t feature_obj_id ,/* <I>
A feature object identifier
*/
int edit ,/* <I>
This is an unused flag. It used to determine whether
to return the right-hand side or both sides of an
expression. Currently, both sides of an expression
are returned.
*/
char ** groove_dia ,/* <OF>
Groove diameter. This must be freed by calling
UF_free.
*/
char ** ball_dia /* <OF>
Ball diameter. This must be freed by calling
UF_free.
*/
);
/********************************************************************
Creates a rectangular groove feature by inputting its location,
direction, diameter and width. Along with these items a placement
face is needed to determine which face the groove is associated to.
The output of this function is the object identifier associated to the
rectangular groove.
Environment: Internal and External
See Also:
The code creates the cylinder
and rectangular groove shown in the preceding figure.
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_create_rect_groove(
double location[3] ,/* <I>
Rectangular groove location.
*/
double direction[3] ,/* <I>
Rectangular groove direction.
*/
char * diame ,/* <I>
Rectangular groove diameter.
*/
char * width ,/* <I>
Rectangular groove width.
*/
tag_t face ,/* <I>
Face for the RPO constraint. The face should be of
type UF_cylinder_type or UF_cone_type.
*/
tag_t * feature_obj_id /* <O>
Feature object identifier of created rectangular
groove
*/
);
/****************************************************************************
Creates a U-groove feature by inputting its location, direction,
diameter, width, and corner radius. Along with these items a
placement face is needed to determine which face the groove is
associated to. The output of this function is the object identifier
associated to the U-groove.
Environment: Internal and External
See Also:
History:
***************************************************************************/
extern UFUNEXPORT int UF_MODL_create_u_groove(
double location[3] ,/* <I>
U groove location.
*/
double direction[3] ,/* <I>
U groove direction.
*/
char * diame ,/* <I>
U groove diameter
*/
char * width ,/* <I>
U groove width.
*/
char * corner ,/* <I>
U groove corner radius
*/
tag_t face ,/* <I>
Face for the RPO constraint.
*/
tag_t * feature_obj_id /* <O>
Feature object identifier of created u-groove
*/
);
#undef EXPORTLIBRARY
#endif /* UF_MODL_GROOVES_H_INCLUDED */