UF_MODL_smhole_data_s (view source)
Defined in: uf_modl_smd.h
Also known as:
- UF_MODL_smhole_data_t
- UF_MODL_smhole_data_p_t
Overview
The following structure is used when creating, editing, or querying a
sheet metal hole.
Data Members
diameter [ UF_MAX_EXP_BUFSIZE ]
char
depth [ UF_MAX_EXP_BUFSIZE ]
char
tip_angle [ UF_MAX_EXP_BUFSIZE ]
char
edge1
offset1 [ UF_MAX_EXP_BUFSIZE ]
char
edge2
offset2 [ UF_MAX_EXP_BUFSIZE ]
char
hole_face
thru_face
datum_axis
method
vec_dir [ 3 ]
double
type