UF_MODL_quilt_data_structures_union (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
This union is used to hold a pointer to one of the previous 5 structures
depending on the type of quilt surface.


Data Members

quilt_type1
UF_MODL_curve_mesh_along_fixed_vector_data_t *


quilt_type2
UF_MODL_curve_mesh_along_driver_normals_data_t *


quilt_type3
UF_MODL_b_surface_along_fixed_vector_data_t *


quilt_type4
UF_MODL_b_surface_along_driver_normals_data_t *


quilt_type5
UF_MODL_self_refit_data_t *