UF_MODL_pocketpad_outline_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
The general pocket/pad functions use this structure to define the
outline to specify the shape of the pocket/pad. This structure also
defines whether the pocket/pad is created with a single outline at
either the placement faces, or the floor/top faces of the pocket/pad, or
with outlines at both the placement faces and the floor/top faces of
the pocket/pad.


Data Members

outline_type
UF_MODL_pocketpad_type_t
Indication of whether the pocket/pad
is being defined with a single
outline at either the placement face
or the floor/top face of the
pocket/pad, or if the pocket/pad is
being defined with outlines at both
the placement face and the floor/top
face of the pocket/pad.
Also controls if the pocket/pad will
be booleaned to a target solid or
not

defined_by
UF_MODL_pocketpad_outline_defined_by_t
The definition of the pocket/pad.